Skip to main content
Md Mubdiul Hasan
Associate III
Dec 29, 2021 2:23 AM UTC
Question

How to change Chineess front in STM32F103

Hi there,

I am handling a project which has display application both for English and Korean front.

I can made some Chineess front/ charecter using Note pad pixel and a software named KSX1001.

May be ASCI II can be generate b16*16 PIXEL image file.

Now its difficuilt to implement those charecter in my front.h file.

For korean laguage its written in the code like,

void TextOut_ASC_II_16(int x, int y, char ch, BOOL bInvert);
void TextOut_Han(int x, int y, char *ch, BOOL bInvert);
void TextOut_ASC_II_8(int x, int y, char ch, BOOL bInvert);
 
void TextOut_5_4(int x, int y, char ch);
 
int TextOut(int x, int y, char *pString, BOOL bInvert);
int TextOut8(int x, int y, char *pString, BOOL bInvert);
 
int TextOut5(int x, int y, char *pString);
 
int DrawText(int x, int y, BOOL bInvert, const char *pcString, ...);
int DrawText8(int x, int y, BOOL bInvert, const char *pcString, ...);
int DrawText8_Right(int x, int y, BOOL bInvert, const char *pcString, ...);
 
void DrawSmallDigit(int x, int y, const char *pcString, ...);
 
void UpdateLCD(void);
 
void DrawXLine(int x, int y, int cx);
void DrawYLine(int x, int y, int cy);
void FillRect(BYTE Left, BYTE Top, BYTE Cx, BYTE Cy);
void DrawBox(int x, int y, int cx, int cy);

In my front.c its written like

const unsigned char IMAGE_8_16[1][16] ( with a row of data)

const unsigned char IMAGE_16_16[COUNT_OF_16_IMAGE][32] ( with a data matrix),,,etc

For korean letter and numbers some charecter with table has been called.

Any idea how to make them ? Is there any global file for it?

This topic has been closed for replies.

3 replies

Peter BENSCH
ST Technical Moderator
Jan 7, 2022 1:43 PM UTC

It looks like you need a converter to convert the fonts (usually vector fonts) into hex codes, which you then convert into a structure.

There are various projects on the internet that have created tools for this, usually closed source, but a few of them free of charge, e.g. TFT Font Factory.

Hope this helps a little?

Good luck!

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Md Mubdiul Hasan
Associate III
Jan 10, 2022 6:16 AM UTC

Thank you sir Peter after a long time.

I can convert them, I have one tool.BMP to front.

But, confused about fully change the front.c file.

Its whole about english and Korean. If I do for cheness then all looks messy.

Associate
Sep 5, 2024 7:30 AM UTC

Are you there sir?