Skip to main content
Associate
Nov 20, 2023 2:12 PM UTC
Solved

How to align(center) two wildcard text areas that change dynamically in the same row?

Hello,

Here is an example of what I am trying to make in TouchGFX Designer.

ex.png

 

 

 

 

 

So, since I need different text colors for text inputs, I am using 2 text area inputs here. Both inputs are wildcards and should change value dynamically. I am having trouble centering them on the screen, as I would like that no matter the length of each value the texts are centered in the container. (like in the attached image).

If I were to present this as one text area with 2 wildcard inputs I would just remove auto-size, expand text area to full width of the container and center it. But here I am using two textareas.

Is there a way to do this in Designer alone or do I need some code added later on to fix the positions?

 

    This topic has been closed for replies.
    ST Employee
    Nov 28, 2023 1:21 PM UTC

    Hello @JJYodd ,

    Unfortunately, there is no direct way to do it in through the designer. However, you can do it in code by getting the width of your text areas, adding them and then substracting from the container's width. Then, by diving by 2, you get the position of your text areas. You get set the position by SetX()
    You can read more about the different functions regarding Drawable here:

    https://support.touchgfx.com/docs/api/classes/classtouchgfx_1_1_drawable

    I hope this help

    Mohammad MORADIST Software Developer | TouchGFX

    3 replies

    ST Employee
    Nov 28, 2023 1:21 PM UTC

    Hello @JJYodd ,

    Unfortunately, there is no direct way to do it in through the designer. However, you can do it in code by getting the width of your text areas, adding them and then substracting from the container's width. Then, by diving by 2, you get the position of your text areas. You get set the position by SetX()
    You can read more about the different functions regarding Drawable here:

    https://support.touchgfx.com/docs/api/classes/classtouchgfx_1_1_drawable

    I hope this help

    Mohammad MORADIST Software Developer | TouchGFX
    JJYoddAuthor
    Associate
    Nov 30, 2023 3:59 PM UTC

    Yes, that is good. Thank you!

    ST Employee
    Dec 5, 2023 3:21 PM UTC

    You are very welcome,

    Good luck 

    Mohammad MORADIST Software Developer | TouchGFX