Skip to main content
MNapi
Senior II
Feb 16, 2019 3:06 PM UTC
Question

how is the Touch GFX supposed to work ?

I see the icon top right corner, generate code. But when I press it nothing happens, it becomes like inactive grayed out like it is doing something for a few seconds but nothing happens.

Is this because used Windows 7, do I need Win 10 ? Is this supposed to generate some initialization code like Cube MX I could use in Keil

I am still using Arduino as my video card for 480x800 display and send data by I2C but I would like eventually get some of the STM32 displays working.

This topic has been closed for replies.

6 replies

Martin KJELDSEN
Principal III
Feb 18, 2019 8:04 AM UTC

Hi @MNapi​,

Which version of TouchGFX are you using? Version 4.10.0 continually generates code based on your Designer Project. The "Generate Code" button is just to show that it's something the designer does and you can execute that function explicitly.

What do you mean by "Nothing happens" ? Are you sure no code was generated? It will be located inside the generated/ folder. It's not generating initialization code, only gui related code. It should work on both Win7 and Win10, no problem.

Let me know!

Best regards,

Martin

MNapi
MNapiAuthor
Senior II
Feb 18, 2019 4:51 PM UTC

I though that it would open some folder to save the project or let me to choose to launch for example Keil. Like it happens in Cube MX.

I have just downloaded the latest Touch GFX it says 4.10.0

I just do not know what the thing is supposed to do or what it is doing. How do I get from Touch GFX to the board.

I would like to get the STM32F769I-DISCO, looks like a nice board with 480x800 display. It does not look to get it ever working with those tools.

Arduino is so simple, with STM32 you need to be a computer scientist.

I got my first STM32F446 about a year ago, you just cannot figure out how to get it working. I only learnt how to program it after watching somebody else youtube videos. From those videos I found how to use CubeMX and Keil, it looks simple now. Those STM manuals are full of assembly language no way you can figure it out unless you are computer scientist.

Tesla DeLorean
Guru
Feb 18, 2019 5:05 PM UTC

>>..unless you are computer scientist.

I'm an Electronics Engineer, and seem to cope.

I thought one of the key selling points of the Cortex-Mx series was the avoidance of assembly language, and the ability to code most everything in C.

I suspect one of the things with Arduino is that it only requires superficial knowledge, rather any of the underlying mechanics, in the same way it is a lot easier to drive cars than fix them.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..