Skip to main content
Human_STM32
Visitor II
Oct 12, 2018 2:41 PM UTC
Question

How do you use control the 7-segment display of the stm32l476-disco board using stm32CubeMX and Kiel?

How do you use control the 7-segment display of the stm32l476-disco board using stm32CubeMX and Kiel? Could someone please help me get a 1 to show on it using this setup?

I am able to successfully control it using either GCC or Keil with the example I found online at http://web.eece.maine.edu/~zhu/book/lab/L4_Lab_02_LCD_C_Driver_Template.zip , but I want to use stm32CubeMX to manage other peripheral ports. Of course this tutorial doesn't use HAL, so it doesn't line up exactly the same.

I have been able to select all the LCD segments in cubemx and compile/upload with Keil5. LED toggles such as PE8 and PB2 work fine. I tried using HAL_GPIO_Toggle for GPIOD15 and Set, for example HAL_GPIO_WritePin(GPIOD, GPIO_BIT_15, GPIO_PIN_SET);

This topic has been closed for replies.

4 replies

T J
Senior III
Oct 12, 2018 9:53 PM UTC

Hey I can help, but I dont have the time... to read..

all the leds are connected to the processor ?

which pins ?

all these pins need to be set to output..

what is 1 ? to show 1, SegB and SegC ?

you need a table, 0 offset gives you the segments you need to show 0.

0 is SegA,B,C,D,E,F = 0x3F

1 is SegB,C = 0x06

2 ...

T J
Senior III
Oct 12, 2018 9:59 PM UTC

dont forget the current limiting resistor... maximum allowed from the processor pin is about 20mA but totally not recommended. less than 1mA is good designing.

I use transistors BC817 and BC807 everywhere...

High currents from the processor pins ( >10mA ) will affect the A/D results,

best to avoid it by using transistor array if needed.

In your case I would use a transistor array. uln2003 was the old favorite

henry.dick
Associate II
Oct 13, 2018 3:23 PM UTC

here is what I use: https://github.com/dannyf00/My-MCU-Libraries---2nd-try

the files are led4_pins.h/.c. they allow the ability to individually assign gpio pins to led pins. and support common cathode or common anode displays, from 1 to 8 digits.

you can easily remap the gpio functions to your favorite library and get it going in no time.

waclawek.jan
Super User
Oct 13, 2018 5:36 PM UTC

The L476 DISCO has a 6-position 14-segment LCD "glass", this is what the OP wants to drive using the on-chip "glass"-LCD controller.

Once the initialization is done, you don't manipulate the indivudual GPIOs, it's the task of the LCD controller. You write to respective positions of LCD_RAM, and then trigger the update by setting LCD_SR.UDR. Further updates are not allowed until the "update done" flag (LCD_SR.UDD) is set. The LCD chapter in RM is relatively clear in this procedure.

There will be probably functions in Cube/HAL for this, I don't Cube/CubeMX. You might want to have a look at the the Demonstration for the 'L476 Disco in Cube to learn how things are used from within Cube - it probably uses [STM32Cube_FW_L4_Vx.xx.x]\Drivers\BSP\STM32L476G-Discovery\stm32l476g_discovery_glass_lcd.c/.h which is where I'd look first.

JW