Skip to main content
HMoon.2
Visitor II
July 14, 2020
Question

How do you create an LCD project for STM32F769I-EAVL in CUBEMX?

Hello

I have a question.

I have STM32F769I-EAVL board.

I can control LCD with TouchGFX.

But I want to create a project and control LCD with CUBEMX.

Is there a tutorial that controls (DSI) LCD through CUBEMX?

If not, could you tell me how to set up CUBEMX and control LCDs?

Thank you.

This topic has been closed for replies.

1 reply

ST Technical Moderator
July 21, 2020

Hello @Community member​ ,

Have a look to AN4860 Application note: DSI Host on STM32F469/479, STM32F7x8/x9 and STM32L4R9/S9 MCUs, which contains : STM32CubeMX configuration example.

A set of example also are provided in STM32CubeF7 firmware package : STM32Cube_FW_F7_V1.16.0\Projects\STM32F769I_EVAL\Examples\LCD_DSI

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks