Skip to main content
MM..1
Super User
February 6, 2022
Question

How create ExtFlashSection bin file only with Simulator project?

We require on one file all images used in gui and address map file for locate images.

Is this possible with simulator TouchGFX project?

This topic has been closed for replies.

2 replies

Romain DIELEMAN
ST Employee
February 8, 2022

Hello MM,

​

Here is what I have been answered by a colleague :grinning_face_with_sweat::

"You can modify the Makefile used by the simulator to produce a binary file with all the images.

It is already done in some of the gcc Makefiles used by the TBS.

Here is a cut from a STM32F746 Makefile:

                     echo "Producing additional output formats..."

                     echo " target.hex  - Combined internal+external hex"

                     $(objcopy) -O ihex $@ $(@D)/target.hex

                     echo " intflash.elf - Internal flash, elf debug"

                     $(objcopy) --remove-section=ExtFlashSection $@ $(@D)/intflash.elf 2>/dev/null

                     echo " intflash.hex - Internal flash, hex"

                     $(objcopy) -O ihex --remove-section=ExtFlashSection $@ $(@D)/intflash.hex

                     # re-enable if extflash binaries are required in your workflow

                     echo " extflash.bin - External flash, binary"

                     $(objcopy) -O binary --only-section=*FlashSection $@ $(@D)/extflash.bin

The last line creates a bin files with all data from the *FlashSections. Here they probably want just the ExtFlashSection.

All images looks like this:

LOCATION_PRAGMA("ExtFlashSection")

KEEP extern const unsigned char image_img1[] LOCATION_ATTRIBUTE("ExtFlashSection") = { // 10x4 RGB888 pixels.

   0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,

   0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,

   0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,

This puts the image data in ExtFlashSection. "

Hope this helps,

/Romain

MM..1
MM..1Author
Super User
February 9, 2022

Hello Romain,

Maybe im noob in edit makefile, but when I place in simulator makefile ...

all: $(filter assets,$(MAKECMDGOALS))

echo " extflash.bin - External flash, binary"

$(objcopy) -O ihex --only-section=*FlashSection $@ $(@D)/extflash.hex

all assets: $(filter clean,$(MAKECMDGOALS))

I get error

Run Simulator

Generate

Done

Generate Assets

make -f simulator/gcc/Makefile assets -j8

simulator/gcc/Makefile:31: *** missing separator. Stop.

Failed

Failed

EDIT1:

I test in command line and too generated makefile and it dont get error, but hex file is empty. Seems simulator exe dont handle sections and in simulator build i dont see file for objcopy.