Skip to main content
DMart.19
Visitor II
Jul 16, 2019 6:46 PM UTC
Question

How connected the physical buffer of the STM32L4R9 discovery board on the external PSRAM (with or without using GFXMMU)?

Hello! Has anyone ever already connected the physical buffer of the STM32L4R9 discovery board on the external PSRAM (with or without using GFXMMU)? All STM32 Cube examples are using a buffer in internal RAM...

When I put the buffer in PSRAM, the rendering on LCD is wrong: some white lines appear and sometimes all the content is wrong.

Actually, I have some LTDC FIFO underrun interrupts. I have follow advices of application note DM00287603.pdf (chapter LTDC required bandwidth) without success. :(

This topic has been closed for replies.

1 reply

STrop
Associate II
Oct 11, 2019 9:12 AM UTC

Hello David,

I currently try to do the same without satisfaction.

Did you manage to put the physical area of GFXMMU to PSRAM ?

Thanks

Simon