Skip to main content
MWasi.11
Associate
October 3, 2020
Question

How connect STM32F4 board with TFT Display using RGB or LVDS interface?

I am using stm32f429 disco board. I want to create a GUI with touchgfx and display it on the external 10.1" tft LCD display

Can anyone tell me how can I connect my stm32f4 board with tft display using RGB or LVDS interface and how to initialize its pins ?

This topic has been closed for replies.

2 replies

ST Technical Moderator
October 7, 2020

Hello @MWasi.1​ ,

You can refer to this AN4861 Application note LCD-TFT display controller (LTDC) on STM32 MCUs, describes the LCD-TFT display controller of the STM32F4 with hardware and pins configurations and application examples.

The ready-to-use examples available in the STM32CubeF4 firmware package can be a starting point:

STM32Cube_FW_F4_V1.25.1\Projects\STM32F429I-Discovery\Examples\LTDC\LTDC_Display_2Layers

STM32Cube_FW_F4_V1.25.1\Drivers\BSP\STM32F429I-Discovery\stm32f429i_discovery_lcd.c

STM32Cube_FW_F4_V1.25.1\Drivers\BSP\Components\ili9341\ili9341.c

Hope this helps you.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
MM..1
Super User
October 7, 2020

I mean 429 have only RGB interface and when you need connect external, you need around 30 lines

Maybe you can use or create reduction FFC cable board , but limit is length

When hw is ready next step is driver to init external display