Skip to main content
egoltzman
Senior
Jun 29, 2019 1:57 PM UTC
Question

How can I use one of the 8BPP format (e.g. ARGB2222)

Hi,

I want to try to use 8BPP in one of the project I'm working on.

I set the LTDC to work in 8BPP and I tried to define a designer project that is configure with 8bpp.

When I try to change the config I get error messages that I can not use this format

This topic has been closed for replies.

1 reply

Martin KJELDSEN
Principal III
Jun 30, 2019 8:29 PM UTC

Hi Eyal,

ARGB2222 (8-bit) is supported in TouchGFX 4.11+. Even though the release is completed and we have the binary, it's not officially released because of internal release dependencies. 4.12 will be out as soon as CubeMX 4.4.0 is released.

/Martin