Skip to main content
ikassma
Associate III
May 18, 2020 9:39 AM UTC
Solved

How can I use Hangul's(Korean) Unicode fonts?

hi dear.

​

I am making a QWERTY Korean input method.

It was confirmed that Unicode is used to express characters using the touchGFX designer. However, Font can only output codes in EUC_KR. In the case of the Korean input method, one code is produced by combining, but one complete code is produced through a combination of 2 to 4 codes. Even during the combination, it is necessary to express the letters, but this is a problem because the entire font of Unicode cannot be output. For example, the word "hoho". When this is input as an input device, the screen output order should be displayed as 'ㅎ'-> '호'-> '홓'-> '호호'. However, '홓' is in the Unicode Font but not in EUC_KR, so it is treated as Blank. How can I solve these problems ????

If you input "홓" in TouchGFX Designer Resource, nothing is displayed.

This topic has been closed for replies.
ikassma
ikassmaBest answer
Associate III
May 18, 2020 11:44 AM UTC

thank for your answer.

I implemented Korean's Automata. Therefore, it is possible to process Unicode for characters being input in the middle. I solved the problem elsewhere. The TTF font I am using does not have some Unicode glyphs. That was the problem and I solved it by changing the TTF font.

2 replies

Martin KJELDSEN
Principal III
May 18, 2020 10:46 AM UTC

TouchGFX is not aware of this. For korean it can only look up unicodes as specified by the text-sheet. If you want to do anything specifically when facing a combination of characters, you'll have to write code to manally pick the ones from the generated font files that you need.

/Martin

ikassma
ikassmaAuthorBest answer
Associate III
May 18, 2020 11:44 AM UTC

thank for your answer.

I implemented Korean's Automata. Therefore, it is possible to process Unicode for characters being input in the middle. I solved the problem elsewhere. The TTF font I am using does not have some Unicode glyphs. That was the problem and I solved it by changing the TTF font.