Skip to main content
Associate
Nov 6, 2023 2:54 AM UTC
Solved

how can I turnoff display backlight led. GFX01M2 Board

I want to program turning on/off display backlight to reduce power consumption.

 

1. how can i turn off / on display backlight led?

2. I use dt022ctft on GFX01M2. 

3. developement board is NUCLEO-G071RB

 

 

    This topic has been closed for replies.
    gbm
    gbmBest answer
    Super User
    Nov 6, 2023 8:49 AM UTC

    Check the schematic. The backlight is permanently connected to power supply via resistor R8, so there is no way to control it. You may modify the board by removing R8 from its position and soldering it in series with an NPN RET (bipolar transistor with build-in resistors, like PDTC series) Another possibility is to use some small NMOSFET, like BSS138, but then you must also add another resistor of 10..100k between gate and ground. You may then control the base/gate of a transistor with some PWM timer output.

    My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

    1 reply

    gbm
    gbmBest answer
    Super User
    Nov 6, 2023 8:49 AM UTC

    Check the schematic. The backlight is permanently connected to power supply via resistor R8, so there is no way to control it. You may modify the board by removing R8 from its position and soldering it in series with an NPN RET (bipolar transistor with build-in resistors, like PDTC series) Another possibility is to use some small NMOSFET, like BSS138, but then you must also add another resistor of 10..100k between gate and ground. You may then control the base/gate of a transistor with some PWM timer output.

    My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice