Skip to main content
YK.10
Associate
Jul 4, 2019 5:52 AM UTC
Question

How can I create interaction if the screens are having only custom containers without any buttons or others?

I am using few custom containers in all the screens I created. I want to make interaction that when i touch one custom container it should take me to that particular screen. But there is no option showing in Trigger. How can i make interaction if the screens are having only custom containers without any buttons or others. Could you please help me out here?

Thanks

Yamuna K

This topic has been closed for replies.

5 replies

Martin KJELDSEN
Principal III
Jul 4, 2019 11:20 AM UTC

The interface for interactions and custom containers has been improved since 4.10. We're working on the next release which will be out with CubeMX 5.4 most likely.

What do your custom containers contain? Do you want to steal the touch for the entire container in order to transition or only parts of it?

/Martin

YK.10
YK.10Author
Associate
Jul 4, 2019 11:56 AM UTC

Each custom container has few images and text. I want the touch option for entire container not part of it for the transition . But it would be appreciated if you guide me to do both.

Thanks,

Yamuna K