Skip to main content
GS1
Senior III
February 24, 2022
Question

How can I copy some elements of a screen from one TouchGFX project to another one with TouchGFX Designer?

I have two projects which are based on TouchGFX. Now I thought I could copy some text, rectangles, lines and button elements from one project to the other one by simply copy and paste within the Designer. But unfortunately this is not working. Does anybody know if there is a way to do this?

BR GS

This topic has been closed for replies.

3 replies

Yoann KLEIN
ST Employee
February 25, 2022

Hello @GS@S​ ,

In TouchGFXDesigner, there is the "Import GUI" tab in the "Edit" menu that enables you to copy the UI from a project to another :

0693W00000KaWhiQAF.png 

Just click that tab and select the project you want to import the UI from.

Hope that that helped you,

/Yoann

Yoann KLEINST Software Developer | TouchGFX
MM..1
Super User
February 26, 2022

Yoann some elements isnt full GUI

DSwea.1
Associate III
March 1, 2022

Agreed. Import replaces the contents of the open project with the contents of the imported project. Copying individual screens and other elements is only possible by tedious and potentially error prone editing of the project's ".touchgfx" file.

Reuse of TouchGFX content is an issue that has been discussed in the forum for several years, but as yet there has been no progress in that area.

See https://community.st.com/s/question/0D53W000019DdGzSAK/how-to-reuse-touchgfx-content, or https://community.st.com/s/question/0D53W00000cSXRrSAO/importexport-custom-container-from-code-files-to-an-other-touchgfx-project