Skip to main content
SSimi.1
Associate II
January 22, 2022
Question

Hi, Is it possible to support 2 brightnesses at the same time with an 8x8 led?

..

    This topic has been closed for replies.

    3 replies

    waclawek.jan
    Super User
    January 23, 2022

    Yes, if you can multiplex fast enough so that two cycles are shorter than the persistence of vision. So, assuming e.g. 100Hz target total "refresh frequency", in plain multiplexing you would have 10ms for one cycle i.e. 1.25ms per row, here you would have 5ms for one one cycle, i.e. 0.625ms per row.

    Then, simply, for half intensity, in one cycle you light up given LED, and in other not.

    JW

    SSimi.1
    SSimi.1Author
    Associate II
    January 23, 2022

    Sry, but that was a little bit too complicated for me, I dont get it

    MM..1
    Super User
    January 23, 2022

    Sorry, but your question is next crystalball ask. Try show schematics...