Skip to main content
Danix2k
Associate III
Jan 3, 2022 10:58 AM UTC
Solved

Hi, I'm using a STM32H757 MCU with a graphical display on my new board. I would like to insert on it a VNC server using TouchGFX tool; is it possible? Thanks.

I saw that with STemWIN library it was possible but is no longer supported on stm32h7 mcu and also in the ST page is reported to use toucgGFX (and stmCube) tools insted STemWIN.

Hou can I add a VNC server module on TouchGFX?

This topic has been closed for replies.
Danix2k
Danix2kBest answer
Associate III
Feb 18, 2022 11:09 AM UTC

Hi,

I asked to STm and no VNC server will be added on touchGFX; for VNC application the user has to insert TCP/IP stack and, after that, create his own VNC application.

3 replies

MM..1
Super User
Jan 3, 2022 2:16 PM UTC

VNC server have nothing with any library. Is network service based on sending copy of framebuffer.

When you implement it you can have

Danix2k
Danix2kAuthor
Associate III
Jan 3, 2022 2:29 PM UTC

With STemWin there was the possibility to activate the VNC Server (there are a lot of example on youtube - internet and also on package for STM32L4) without implementing the VNC protocol by yourself. Now, on touchGFX, or better, STM32CubeMX it seems that there is no "middleware" to enable this feature if I'm using CubeGFX

Danix2k
Danix2kAuthorBest answer
Associate III
Feb 18, 2022 11:09 AM UTC

Hi,

I asked to STm and no VNC server will be added on touchGFX; for VNC application the user has to insert TCP/IP stack and, after that, create his own VNC application.