Skip to main content
JHeyd.1
Associate
October 7, 2020
Question

Hello I have a problem with my discovery bord "STM32F469I-DISCOVERY" when I use TouchGFX Designer and I only create a box (background) and a text area:

When I execute "run target" the compilation and flashing is successfully but I see nothing on the display of the board. When I do the same with simulator or with STM32CubeIDE everything is visible. The strange thing is when I add a button to my screen I also see the whole things on display of board when I execute "run target".

So for me it seems that this issue seems to be compiler dependant.

Thanks in advance for helping

Best regards

Jürgen

This topic has been closed for replies.

2 replies

Uusta.1
Associate III
January 27, 2022

Hi Jürgen, did you solve this problem? I'm facing same problem too when I try to use with NO OS on my stm32f469i-disco board

Romain DIELEMAN
ST Employee
January 27, 2022

On this specific post I wonder if all the correct changes were made in the Makefile in the /gcc folder (which is used by the "run target" button)

/Romain