Skip to main content
Ali1
Visitor II
October 12, 2021
Question

Hello, I am a newbie.I am building a UI simple one using the board STM32H7B3DK. When i run the simulator it gives the following error. Could anyone please help in this case. There is also error when i flash UI on board. I double check the board i sel

Run Simulator

   Generate

       Done

   Generate Assets

       make -f simulator/gcc/Makefile assets -j8

       Reading ./application.config

       Done

   Post Generate

       touchgfx update_project --project-file=simulator/msvs/Application.vcxproj

       Done

   Post Generate Target

       touchgfx update_project --project-file=../STM32H7B3I-DK.ioc --platform=m7

       .project files generated inside project folder

       This is STM32CubeIDE project updater: Working on ../STM32CubeIDE/.project

       Project file: ../STM32CubeIDE/.cproject

       Done

   Compile

       make -f simulator/gcc/Makefile -j8

       Reading ./application.config

       Compiling gui/src/screen1_screen/Screen1Presenter.cpp

       Compiling gui/src/screen1_screen/Screen1View.cpp

       Compiling generated/gui_generated/src/screen1_screen/Screen1ViewBase.cpp

       Compiling generated/gui_generated/src/common/FrontendApplicationBase.cpp

       Compiling generated/simulator/src/mainBase.cpp

       Compiling generated/images/src/image_router.cpp

       Compiling simulator/main.cpp

       cc1plus.exe: out of memory allocating 1073745919 bytes

       make[2]: *** [build/MINGW32_NT-6.2/generated/images/src/image_router.o] Error 1

       generated/simulator/gcc/Makefile:190: recipe for target 'build/MINGW32_NT-6.2/generated/images/src/image_router.o' failed

       generated/simulator/gcc/Makefile:149: recipe for target 'generate_assets' failed

       make[1]: *** [generate_assets] Error 2

       simulator/gcc/Makefile:32: recipe for target 'all' failed

       make: *** [all] Error 2

       Failed

   Failed

This topic has been closed for replies.