Skip to main content
HBalo.1
Associate
Aug 24, 2020 11:29 AM UTC
Question

hello guys. i work with touch GFX but i have a question. can i startup a 7" LCD with stm32f469i eval? if yes how?

and more, how the characteristic parameter this LCD has?

This topic has been closed for replies.

4 replies

Alexandre RENOUX
Visitor II
Aug 24, 2020 1:43 PM UTC

Hello,

What is this 7'' LCD ? Because it's not the one embedded on the F469-EVAL.

Please provide more information.

/Alexandre

HBalo.1
HBalo.1Author
Associate
Aug 30, 2020 5:48 PM UTC

In fact, I designed my work in touchgfx software on stm32f469 eval.

Now if I design a board exactly like the stm32f469 eval board and put a 7-inch lcd with a resolution of 480 x 800 on it, according to the touchgfx settings, will the code generated by touchgfx run on this hardware?

And my question is exactly what 7-inch LCD should I get so that I do not get into trouble?

Will the problem be solved just by changing the settings of the LTDC unit according to the 7-inch LCD?

Alexandre RENOUX
Visitor II
Sep 7, 2020 7:04 AM UTC

Hello,

Yes in theory the code generated by CubeMX and TouchGFX should work.

For the screen, we don't have any recommendation in particular. If you choose a LTDC screen, this will simplify the implementation as LTDC is fully handled by TouchGFX Generator.

/Alexandre

mehmet06
Associate
Mar 12, 2024 1:26 PM UTC

I want to use a 7 inch and above screen with toucgfx and you do not know which screen I can use. So what use will this kit be if I can't make an original design and I can't even find the screen on it? I paid a ton of money for the stm32f469 i kit.