Skip to main content
YH.1
Associate
May 30, 2021
Solved

Hello, everyone. I puzzle over the LCD alternative function of stm32F429VI.

According to the datasheet, F429​VI has no pin for LCD_R0, LCD_R1 andLCD_B1. does it mean the chip doesn't support 24bits colors (I don't want to use FMC instead of LCD-TFT)?

​

(the F429 with more pins has all of the color pins, according to the pin definitions )

This topic has been closed for replies.
MM..1
MM..1Best answer
Super User
May 30, 2021

Yes this package is good for displays with RGB666 , but support 24bit for example over SPI.

2 replies

MM..1
MM..1Best answer
Super User
May 30, 2021

Yes this package is good for displays with RGB666 , but support 24bit for example over SPI.

YH.1
YH.1Author
Associate
May 30, 2021

Thanks!​