Skip to main content
February 5, 2021
Solved

Have anybody QSPI loader algorythm for Keil?

Have anybody QSPI loader algorythm for Keil?

I can't create workable code....

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
February 5, 2021

https://www.keil.com/pack/Keil.STM32H7xx_DFP.2.7.0.pack

Tip: It's a .ZIP file...

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

12 replies

MM..1
Super User
February 5, 2021

When you have installed stlink utility try read readme.txt in

c:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader\MX25LM51245G_STM32L4R9I-DISCO 

here exist too keil project...

February 5, 2021

thanks for link, a used this sample when I worked with F746 and w25q - without problems.

But H743 and MT25QL.......

void QSPI_WriteEnable(void)
{
 QUADSPI_ComConfig_InitTypeDef QUADSPI_ComConfig_InitStructure;
	
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_FMode = QUADSPI_ComConfig_FMode_Indirect_Write;
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_DDRMode = QUADSPI_ComConfig_DDRMode_Disable;
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_SIOOMode = QUADSPI_ComConfig_SIOOMode_Disable;
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_DummyCycles = 0;
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_ABSize = QUADSPI_ComConfig_ABSize_8bit;
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_ADSize = QUADSPI_ComConfig_ADSize_24bit;
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_DMode = QUADSPI_ComConfig_DMode_NoData;
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_ADMode = QUADSPI_ComConfig_ADMode_NoAddress;
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_ABMode = QUADSPI_ComConfig_ABMode_NoAlternateByte;
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_IMode = QUADSPI_ComConfig_IMode_1Line;
 
 
 
 QUADSPI_SetFIFOThreshold(0);
 QUADSPI_SetDataLength(0);
 
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_Ins = WRITE_ENABLE_CMD ; 
 QUADSPI_ComConfig_Init(&QUADSPI_ComConfig_InitStructure);
 while(QUADSPI_GetFlagStatus(QUADSPI_FLAG_BUSY)==SET);
 
sprintf((char *)str, "WR1: 0x%08X \r\n ",QUADSPI_GetFMode());
 
			 HAL_UART_Transmit(&huart7, str, strlen((char *)str), 3000); 
 
 
 QUADSPI_AutoPollingMode_Config(0x02,0x02,QUADSPI_PMM_AND);
 QUADSPI_AutoPollingModeStopCmd(ENABLE);
 QUADSPI_SetDataLength(0x00);
 
 
 
 
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_FMode = QUADSPI_ComConfig_FMode_Auto_Polling;
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_ADMode = QUADSPI_ComConfig_ADMode_NoAddress;
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_DMode = QUADSPI_ComConfig_DMode_1Line;
 QUADSPI_ComConfig_InitStructure.QUADSPI_ComConfig_Ins = READ_STATUS_REGISTER_CMD;
 QUADSPI_ComConfig_Init(&QUADSPI_ComConfig_InitStructure); 
 
sprintf((char *)str, "WR2: 0x%08X \r\n ",QUADSPI_GetFMode());
 
			 HAL_UART_Transmit(&huart7, str, strlen((char *)str), 3000); 
 
 
 while(QUADSPI_GetFlagStatus(QUADSPI_FLAG_SM)==RESET);
	
	
 QUADSPI_ClearFlag(QUADSPI_FLAG_SM);
 QUADSPI_ClearFlag(QUADSPI_FLAG_TC);
 while(QUADSPI_GetFlagStatus(QUADSPI_FLAG_BUSY)==SET);
	
	sprintf((char *)str, "WR3: 0x%08X \r\n ",QUADSPI_GetFMode());
 
			 HAL_UART_Transmit(&huart7, str, strlen((char *)str), 3000); 
 
}

it halts on

 while(QUADSPI_GetFlagStatus(QUADSPI_FLAG_SM)==RESET);
	

February 5, 2021

I want for STM32H743 and MT25QL

Tesla DeLorean
Guru
February 5, 2021

On what pins? Don't they have some in the "Packs" directories for the H7 related to the EVAL or DISCO boards?

C:\Keil5xx\Arm\Packs\Keil\STM32H7xx_DFP\2.7.0\CMSIS\Flash\STM32H747I_Disco_QSPI\QSPI

C:\Keil5xx\Arm\Packs\Keil\STM32H7xx_DFP\2.7.0\CMSIS\Flash\STM32H7xx_MT25TL01G.FLM

The QL's should be a relatively short walk

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
February 5, 2021

Your second link is for MT25TL01G, but I have MT25QL128

Yor first link - my DFP version is 2.4.0, updater list contains onl 2.5.1. Where you got 2.7.0 version?

Folder STM32H747IDisco_QSPI\QSPI contains SOURCE or .FLM?