Skip to main content
YMaha
Associate
Jul 18, 2019 7:18 AM UTC
Question

Has anyone used STM32F769I Discovery Board with the 10 inch display and capacitive touch screen and coded the system in TouchGFX? Can you please tell me make of such display which will be compatible with STM32F769I-DISCO1 and TouchGFX?

..

This topic has been closed for replies.

2 replies

Mon2
Senior III
Jul 18, 2019 10:37 AM UTC

Can you post more details on which Discovery Board you are referencing? The STM32F769I Discovery Board by ST is supplied by a 4" DSI interface LCD panel with a capacitive touch screen (CTP).

YMaha
YMahaAuthor
Associate
Jul 18, 2019 12:03 PM UTC

Correct, STM32F769I-DISCO is provided with 4" DSI LCD panel and CTP.

However, I want to replace this 4" display with the 10" LCD panel also with CTP.

If there is any readily available 10" display directly compatible with STM32F769I is what I wanted to know.