Has anyone successfully used RTOS and STemWin with CubeMX and SW4STM?
- 1 reply
- 1079 views
Hello all.
We have STemWin properly running on STM32L4R7, but STemWin uses quite a large amount of CPU time to draw display contents etc. We cannot allow that, because we have a time critical task to do (RealTime). So the sollution would be: use RTOS.
We managed to setup RTOS nicely, switching between tasks by using "osDelay" works fine. But when we add STemWin the Gui_Exec takes quite long and needs to be interrupted by preeption. When this occurs, the PendSV Handler the instruction "ldmia.w r0!,{R4-R11,R14} crashes and jumps into the hard fault handler.
Has anyone successfully used RTOS and STemWin with preemption on STM32L4Rx ?
Thanks for any help.
Attached project is generated with CubeMX5.2.1 for SW4STM
We use an FMC based Display.
We didn't do anything fancy. We just configured the project with CubeMX. All libs and settings are provided by CubeMX Code Generation.
Johannes
PendSV_Handler:
08004e10: mrs r0, PSP
08004e14: isb sy
08004e18: ldr r3, [pc, #84] ; (0x8004e70 <PendSV_Handler+96>)
08004e1a: ldr r2, [r3, #0]
08004e1c: tst.w lr, #16
08004e20: it eq
08004e22: vstmdbeq r0!, {s16-s31}
08004e26: stmdb r0!, {r4, r5, r6, r7, r8, r9, r10, r11, lr}
08004e2a: str r0, [r2, #0]
08004e2c: stmdb sp!, {r0, r3}
08004e30: mov.w r0, #80 ; 0x50
08004e34: msr BASEPRI, r0
08004e38: dsb sy
08004e3c: isb sy
08004e40: bl 0x800484c <vTaskSwitchContext>
08004e44: mov.w r0, #0
08004e48: msr BASEPRI, r0
08004e4c: pop {r0, r3}
08004e4e: ldr r1, [r3, #0]
08004e50: ldr r0, [r1, #0]
08004e52: ldmia.w r0!, {r4, r5, r6, r7, r8, r9, r10, r11, lr}