Skip to main content
PPres
Associate
Jan 26, 2021 6:04 PM UTC
Question

Hardfault when call setTypedText

Hi,

I'm developing on a custom hardware, trying to run a simple touchgfx project.

Single screen with an image an a text over.

Following the example and the strusture of a STM32F746G-Disco demo board, I makemy hardware functioning, any image, even big goes on the 800x480 LCD.

But any time I try to put on the screen a text the system faut to Hrdfault handler.

it seem that the function trying to call a protected area ( 0x5xxxxxx) .

I get that problem every time I try to call "setTypedText" funcion.

I don't understand if some memory settings in my app is wrong. I did try to put the text into external or internal memory, using wildcards or not. It's impossible to show any text.

I use freertos, the project is created with CubeMX + Touchgfx Designer.

I did encrease the heap and the stack.

Nothing. several images at the same time pass the test, but no text even if I use a single font and try printing a single word.

Please point me in some direction to search.

Thanks.

Paolo

This topic has been closed for replies.

18 replies

MSecr.1
Associate II
Jul 10, 2024 10:49 AM UTC

I was facing that specific issue due to a stack overflow, so make sure you allocated enough memory for the stack