Skip to main content
Associate
Sep 9, 2024 8:45 AM UTC
Solved

Hardfault on STM32F769 using TouchGFX

hi

I use touchgfx 4.24 , STM32CubeIDE 1.16 and STM32cubeMX 6.12

I do a project with touchgfx, I import it on cubeide, no problems to launch it on the card (STM32F769I-DISCO)

I make a modification ( uart 5) on the file ioc and the bilioteque (newlib rentrand) as requested by CubeMX. When I launch after compilation I have an error, of type MemManage_Handler
I do not see mistake that I could have comeate.
Who can help me?

thank

This topic has been closed for replies.
GaetanGodart
GaetanGodartBest answer
ST Employee
Sep 23, 2024 9:27 AM UTC

Hello @pascalous ,

 

I would guess it is an issue with FreeRTOS actually.

Can you try to activate your UART5, but when do not fix the warning about NEWLIB_REENTRANT, when STM32CubeMX asks you "Do you still want to generate code", just click "Yes".

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)

16 replies

mƎALLEm
ST Technical Moderator
Sep 9, 2024 10:21 AM UTC

Hello @pascalous and welcome to the community,

Check the MPU config and if you declared something in a memory region that MPU prevents that access.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
pascalousAuthor
Associate
Sep 9, 2024 11:28 AM UTC

thank for reply

I just remade a project, I neither is put any personal code. I put uart5 in assynchrone mode, I complicate the file ioc and I have the same problem. uart5 and mpu have they the same memory zone?

 

mƎALLEm
ST Technical Moderator
Sep 9, 2024 11:32 AM UTC

Before enabling the UART, did you get the same behavior?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
pascalousAuthor
Associate
Sep 9, 2024 11:31 AM UTC

sorry

i build ioc....not complicate

pascalousAuthor
Associate
Sep 9, 2024 5:07 PM UTC

sorry for my mistake

I've just send you the complet project

thank you for help

 

 

mƎALLEm
ST Technical Moderator
Sep 10, 2024 9:49 AM UTC

Hello @pascalous and thank you for the sharing.

I reproduced the behavior and seems doesn't have a link to USART activation but to the TouchGFX task itself.

Attached your project where I commented out all the code not related to the TouchGFX, increased the Stack size, optimization to None. Still having the issue. Checked MPU config, I don't see any issue 

I think better to move this topic to TouchGFX forum so TouchGFX team can help you.

@GaetanGodart, could you help on this topic?

Thank you.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
pascalousAuthor
Associate
Sep 10, 2024 12:10 PM UTC

Thank you for your return, SofLit

pascalousAuthor
Associate
Sep 20, 2024 8:16 AM UTC

hi

update perform the issue persists
I can’t use my STM32F769I-DISCO card with wifi module and touchgfx
Is there another method?

 

GaetanGodart
GaetanGodartBest answer
ST Employee
Sep 23, 2024 9:27 AM UTC

Hello @pascalous ,

 

I would guess it is an issue with FreeRTOS actually.

Can you try to activate your UART5, but when do not fix the warning about NEWLIB_REENTRANT, when STM32CubeMX asks you "Do you still want to generate code", just click "Yes".

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
pascalousAuthor
Associate
Sep 25, 2024 12:28 PM UTC

It works, thank you for your help

GaetanGodart
ST Employee
Sep 25, 2024 12:53 PM UTC

I am glad it fixed your issue! :smiling_face_with_smiling_eyes:

Gaetan GodartSoftware engineer at ST (TouchGFX)