Skip to main content
Associate
Mar 26, 2025 2:28 PM UTC
Question

HardFault in TouchGFX Default Project on STM32H7S78-DK

Hello,

I am using a STM32H7S78-DK and I created a project using TouchGFX Designer with the default empty template. However, when I try to run it, the board immediately hard faults.

Stack Trace:

main()
└── MX_TouchGFX_Init()
└── touchgfx_components_init()
└── nema_init()
└── nema_sys_init()
└── tsi_malloc_init_pool_aligned(1, (void*)nemagfx_stencil_buffer_mem, (uintptr_t)nemagfx_stencil_buffer_mem, NEMAGFX_STENCIL_POOL_SIZE, 1, 8);

I've seen some some discussions where the CRC could be the problem, everything seems fine with the CRC, and i don't think any of the issues are directly related to the NeoChrom GPU.
A while back i tried the same project setup, and it was fine. After that i was checking Rust with Embassy and adding lvgl to an empty project. I'm not sure if it could be related, it might just be a weird coincidence.

This topic has been closed for replies.

6 replies

GaetanGodart
ST Employee
Mar 26, 2025 3:12 PM UTC

Hello @diogomargalho ,

 

Can you describe the steps to achieve this error?

I open TouchGFX Designer 4.25.0, create a new project with STM32H7S78-DK with freeRTOS and RGB565 and I am able to flash from the TouchGFX Designer itself.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
Associate
Mar 26, 2025 4:04 PM UTC

The steps to achieve it are:

  1. Open TouchGFX Designer.
  2. Create 'STM32H7S78 Discovery Kit'
  3. Generate Code
  4. Open the project with STM32CubeIDE
  5. Add the Boot ELF to the Application Startup
    diogomargalho_0-1743004526681.png
  6. Debug 'STM32H7S78-DK_Appli'

After this it crashes.

Debug window

diogomargalho_2-1743004788128.png

Fault Analyzer window

diogomargalho_3-1743004833294.png

nema_hal.c file

diogomargalho_4-1743004990113.png

 



GaetanGodart
ST Employee
Mar 26, 2025 5:18 PM UTC

I never flashed a STM32H7S78-DK through STM32CubeIDE.

Usually, I build the code through STM32CubeIDE and then I open STM32CubeProgrammer to flash.
I select the external loader for the STM32H7S78-dk board then I connect the board, then I flash the boot and then I flash the appli.

Would this be ok for you to do that or do you really want to flash through STM32CubeIDE (I am not an expert on STM32CubeIDE but I could ask someone).

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)