Skip to main content
LMI2
Senior III
Mar 25, 2019 8:34 PM UTC
Question

Hard fault from full screen jpg images with STM32F746 Discovery

Smaller images work now but when I try full screen images, I get a hard fault. I have changed dimension in main.h.

I have used code from repository/application with small modifications

FATFS SDFatFs; /* File system object for SD card logical drive */
FIL MyFile; /* File object */
char SDPath[4]; /* SD card logical drive path */
RGB_typedef *RGB_matrix; 
uint8_t _aucLine[2048];
//uint8_t _aucLine[4048];
uint32_t offset = 0;
//uint32_t line_counter = 239;
uint32_t line_counter = 271;
/* Private function prototypes -----------------------------------------------*/
static void SystemClock_Config(void);
static void LCD_Config(void);
static uint8_t Jpeg_CallbackFunction(uint8_t* Row, uint32_t DataLength);
static void CPU_CACHE_Enable(void);
 
/* Private functions ---------------------------------------------------------*/
 
/**
 * @brief Main program
 * @param None
 * @retval None
 */
int main(void)
{
 /* Enable the CPU Cache */
 CPU_CACHE_Enable();
 
 /* STM32F7xx HAL library initialization:
 - Configure the Flash ART accelerator on ITCM interface
 - Systick timer is configured by default as source of time base, but user 
 can eventually implement his proper time base source (a general purpose 
 timer for example or other time source), keeping in mind that Time base 
 duration should be kept 1ms since PPP_TIMEOUT_VALUEs are defined and 
 handled in milliseconds basis.
 - Set NVIC Group Priority to 4
 - Low Level Initialization
 */
 HAL_Init();
 
 /* Configure the system clock to 200 MHz */
 SystemClock_Config();
 
 /*##-1- LCD Configuration ##################################################*/ 
 LCD_Config();
//offset = 0;
//line_counter = 271;
 if(FATFS_LinkDriver(&SD_Driver, SDPath) == 0)
 {
 
 if(f_mount(&SDFatFs, (TCHAR const*)SDPath, 0) == FR_OK)
 {
 while (1)
{
 if(f_open(&MyFile, "leif.jpg", FA_READ) == FR_OK)
 {
 }
			 jpeg_decode(&MyFile, IMAGE_WIDTH, _aucLine, Jpeg_CallbackFunction);
			 	HAL_Delay(2000);
 offset = 0;
line_counter = 271;
			 if(f_open(&MyFile, "61.jpg", FA_READ) == FR_OK)
 {
 }
			 		jpeg_decode(&MyFile, IMAGE_WIDTH, _aucLine, Jpeg_CallbackFunction);
			 	HAL_Delay(2000);
			 offset = 0;
line_counter = 271;
 }
	 }
 }
		 f_close(&MyFile);
}

This topic has been closed for replies.

3 replies

Bob S
Super User
Mar 25, 2019 9:02 PM UTC

As is the answer to most all questions about "why does my code hard fault" - Add code or otherwise set a breakpint in your hard fault handler. Then look at the fault registers to see what triggered the fault. It should lead you to a program counter value or memory address value. That have been several threads on this forum about this.

LMI2
LMI2Author
Senior III
Mar 26, 2019 7:24 AM UTC

Is it even possible to show full screen jpg images with STM32F746 Discovery.

By the way, does the code in the code window really look this bad. Lines wrap randomly and not much formatting left.

Tesla DeLorean
Guru
Mar 27, 2019 12:31 AM UTC

I would expect the decoder to be pipelined, and be able to accept and output smaller pieces.

Perhaps use a Hard Fault Handler and pin down what code specifically is faulting.

Make sure the buffers are sufficiently large, and whether the faulting code is bad, or if it has been given data/variables/pointers corrupted by a decode operation.

HardFault_Handler\
 PROC
 EXPORT HardFault_Handler
 
 ; Determine correct stack
 
 TST lr, #4
 ITE EQ
 MRSEQ R0, MSP ; Read MSP (Main)
 MRSNE R0, PSP ; Read PSP (Process)
 
 MOV R1, R4 ; Registers R4-R6
 MOV R2, R5
 MOV R3, R6 ; sourcer32@gmail.com
 
 EXTERN hard_fault_handler_c
 B hard_fault_handler_c
 
 ENDP ; HardFault_Handler
 
 
void hard_fault_handler_c(unsigned int * hardfault_args, unsigned int r4, unsigned int r5, unsigned int r6)
{
 printf ("\n[Hard Fault]\n"); // After Joseph Yiu
 
 printf ("r0 = %08X, r1 = %08X, r2 = %08X, r3 = %08X\n",
 hardfault_args[0], hardfault_args[1], hardfault_args[2], hardfault_args[3]);
 printf ("r4 = %08X, r5 = %08X, r6 = %08X, sp = %08X\n",
 r4, r5, r6, (unsigned int)&hardfault_args[8]);
 printf ("r12= %08X, lr = %08X, pc = %08X, psr= %08X\n",
 hardfault_args[4], hardfault_args[5], hardfault_args[6], hardfault_args[7]);
 
 printf ("bfar=%08X, cfsr=%08X, hfsr=%08X, dfsr=%08X, afsr=%08X\n",
 *((volatile unsigned int *)(0xE000ED38)),
 *((volatile unsigned int *)(0xE000ED28)),
 *((volatile unsigned int *)(0xE000ED2C)),
 *((volatile unsigned int *)(0xE000ED30)),
 *((volatile unsigned int *)(0xE000ED3C)) );
 
 while(1);
}

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..