Skip to main content
dgiovanelli
Associate III
Nov 8, 2019 4:55 PM UTC
Question

HAL_DCMI_FrameEventCallback not called in snapshot mode

Hello,

I'm having problems in getting the HAL_DCMI_FrameEventCallback called from the HAL layer.

I'm using the DCMI in snapshot mode and from what I understood reading the dcmi hal driver code, the frame interrupt for snapshot mode is enabled when the DCMI_IT_FRAME is disabled. This looks weird but this is what the next code (line 1305 to 1334 of stm32l4xx_hal_dcmi.c) seems to do. I suppose there is a reason for this.

/* if End of frame IT is disabled */
 if((hdcmi->Instance->IER & DCMI_IT_FRAME) == 0x0U)
 {
 /* If End of Frame flag is set */
 if(__HAL_DCMI_GET_FLAG(hdcmi, (uint32_t)DCMI_FLAG_FRAMERI) != 0x0UL)
 {
 /* Clear the End of Frame flag */
 __HAL_DCMI_CLEAR_FLAG(hdcmi, DCMI_FLAG_FRAMERI);
 
 /* When snapshot mode, disable Vsync, Error and Overrun interrupts */
 if((hdcmi->Instance->CR & DCMI_CR_CM) == DCMI_MODE_SNAPSHOT)
 {
 /* Disable the Vsync, Error and Overrun interrupts */
 __HAL_DCMI_DISABLE_IT(hdcmi, DCMI_IT_LINE | DCMI_IT_VSYNC | DCMI_IT_ERR | DCMI_IT_OVR);
 
 hdcmi->State = HAL_DCMI_STATE_READY;
 
 /* Process Unlocked */
 __HAL_UNLOCK(hdcmi);
 }
 
 /* Frame Event Callback */
#if (USE_HAL_DCMI_REGISTER_CALLBACKS == 1)
 /*Call registered DCMI frame event callback*/
 hdcmi->FrameEventCallback(hdcmi);
#else
 HAL_DCMI_FrameEventCallback(hdcmi);
#endif /* USE_HAL_DCMI_REGISTER_CALLBACKS */
 }
 }

However, the HAL_DCMI_FrameEventCallback never gets called from that code regardless the status of DCMI_IT_FRAME. Moreover, if I run the code in debug mode and I place a breakpoint and then I go on step-by-step, the execution goes to HAL_DCMI_FrameEventCallback which is called as expected.

So, how I get HAL_DCMI_FrameEventCallback called in snapshot mode?

Thank you,

Davide.

PS: The image is small (less than 65535 words)

This topic has been closed for replies.

1 reply

Patrick Chwalek
Associate III
Apr 6, 2022 10:15 PM UTC

Did you ever figure this out? I ran into the same issue. I'm wondering if it's some issue specific to certain cameras where ST's HAL doesn't properly detect the end-of-frame.