Skip to main content
Vlaty.1
Associate III
June 18, 2021
Solved

Good afternoon, In I have two projects Your JPEG_DecodingFs_DMA and mine. In your project, after executing the HAL_JPEG_Decode_DMA function in normal mode, the function returns 4110 bytes of Context in a stepwise 14 bytes. In my program, the HAL_JPEG

Good afternoon, In I have two projects Your JPEG_DecodingFs_DMA and mine. In your project, after executing the HAL_JPEG_Decode_DMA function in normal mode, the function returns 4110 bytes of Context in a stepwise 14 bytes. In my program, the HAL_JPEG_Decode_DMA function always returns 14 bytes. What settings are responsible for setting HAL_JPEG_Decode_DMA()? Sincerely, Alexander.

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
June 18, 2021

Hello @Vlaty.1​ ,

Have a look at this AN4996 Application note Hardware JPEG codec peripheral in STM32F76/77xxx and STM32H743/53/45/55/47/57/50/A3/B3/B0xx microcontrollers.

This application note will help you on the JPEG settings for JPEG decoding applications.

Hope this helps you!

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Imen.DBest answer
ST Technical Moderator
June 18, 2021

Hello @Vlaty.1​ ,

Have a look at this AN4996 Application note Hardware JPEG codec peripheral in STM32F76/77xxx and STM32H743/53/45/55/47/57/50/A3/B3/B0xx microcontrollers.

This application note will help you on the JPEG settings for JPEG decoding applications.

Hope this helps you!

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Vlaty.1
Vlaty.1Author
Associate III
June 21, 2021

Good afternoon. Thanks. It worked. Sincerely, Alexander.