Skip to main content
ferro
Lead
Oct 17, 2025 11:06 AM UTC
Question

GfxDesigner : how to terminate the build process

Hi,

I’d like to terminate the build process, but pressing F7 causes GfxDesigner(4.24.1) to crash.

2025-10-17 13:46:51,280 [1] WARN TouchGFXDomainModel.Texts.FontGetter: font already added. (path: HPSimplified_LtIt.ttf, name: HPSimplified_LtIt
2025-10-17 13:46:51,280 [1] WARN TouchGFXDomainModel.Texts.FontGetter: font already added. (path: HPSimplified_Rg.ttf, name: HPSimplified_Rg
2025-10-17 13:48:35,702 [26] ERROR TouchGFXDesigner.App: Invalid class 
System.Management.ManagementException: Invalid class 
 at System.Management.ManagementException.ThrowWithExtendedInfo(ManagementStatus errorCode)
 at System.Management.ManagementObjectCollection.ManagementObjectEnumerator.MoveNext()
 at TouchGFXApplication.Executors.Executor.Cancel()
 at TouchGFXApplication.MonitorCommands.RunSimulatorCommand.Cancel()
 at TouchGFXApplication.TouchGFXApplication.<CancelCompile>b__38_0()
 at System.Threading.ExecutionContext.RunInternal(ExecutionContext executionContext, ContextCallback callback, Object state)
--- End of stack trace from previous location ---
 at System.Threading.ExecutionContext.RunInternal(ExecutionContext executionContext, ContextCallback callback, Object state)

Is there any other way to do that ? A key combination ?

Thanks

ferro_1-1760699067741.png

 

ferro_0-1760699027631.png

 

    This topic has been closed for replies.

    2 replies

    ST Technical Moderator
    Oct 20, 2025 8:23 AM UTC

    Hello @ferro.

    I am not aware of any other way to terminate the build except by pressing Cancel or F7 without closing TouchGFX Designer. However, I have never experienced issues with this.

    Does the issue only occur when you cancel the simulator build, or does it also happen with Generate Code and Run Target (if available)? Could you try to replicate the issue in TouchGFX 4.26.0?

    Best regards,
    Johan

    ferro
    ferroAuthor
    Lead
    Oct 20, 2025 7:19 PM UTC

    Thanks @JohanAstrup 

    With 4.24.1, I press F5 and the Designer starts to generate code. Pressing F7 during that causes the Designer to crashe. So it does when I press F7 while compiling. I run simulation only.

    "Could you try to replicate the issue in TouchGFX 4.26.0?"

    I will.