Skip to main content
ferro
Lead
Mar 4, 2025 6:02 PM UTC
Solved

GfxDesigner: add menu option 'Code > Build Code'

Hi Gfx Team,

Could you consider adding an option to build code without running.

ferro_0-1741111273154.png

Thanks

    This topic has been closed for replies.
    GaetanGodart
    GaetanGodartBest answer
    ST Employee
    Mar 5, 2025 9:29 AM UTC

    Hello @ferro ,

     

    I don't think we will implement this functionality because you can simply click the Program and Run Target button (bottom right) and not connect your board so that it will compile the code but fail at the beginning of the flashing process.
    The processes are Generate, Generate assets (sometimes the longest), Post generate, Post generate target, Compile (often the longest), Flash.
    If you do not connect a board, STM32CubeProgrammer will not be able to find a STLink connected and the flashing step will quickly fail :

    Flash
     make -f ../../gcc/Makefile flash
     make -C PATHTOTHEPROJECT/MyApplication/gcc/ --no-print-directory -f makefile_boot flash
     Linking Boot/TouchGFX/build/bin/target.elf
     Producing additional output formats...
     target.hex - Combined internal+external hex
     intflash.elf - Internal flash, elf debug
     intflash.hex - Internal flash, hex
     -------------------------------------------------------------------
     STM32CubeProgrammer v2.18.0 
     -------------------------------------------------------------------
     
     Error: No debug probe detected.
     PATHTOTHEPROJECT/MyApplication/gcc/include/flash_sections_int_ext.mk:10: recipe for target '_intflash_' failed
     make[2]: *** [_intflash_] Error 1
     makefile_boot:45: recipe for target 'flash' failed
     make[1]: *** [flash] Error 2
     ../../gcc/Makefile:8: recipe for target 'flash' failed
     make: *** [flash] Error 2
     Failed
     Failed

     

    Regards, 

    Gaetan GodartSoftware engineer at ST (TouchGFX)

    9 replies

    GaetanGodart
    GaetanGodartBest answer
    ST Employee
    Mar 5, 2025 9:29 AM UTC

    Hello @ferro ,

     

    I don't think we will implement this functionality because you can simply click the Program and Run Target button (bottom right) and not connect your board so that it will compile the code but fail at the beginning of the flashing process.
    The processes are Generate, Generate assets (sometimes the longest), Post generate, Post generate target, Compile (often the longest), Flash.
    If you do not connect a board, STM32CubeProgrammer will not be able to find a STLink connected and the flashing step will quickly fail :

    Flash
     make -f ../../gcc/Makefile flash
     make -C PATHTOTHEPROJECT/MyApplication/gcc/ --no-print-directory -f makefile_boot flash
     Linking Boot/TouchGFX/build/bin/target.elf
     Producing additional output formats...
     target.hex - Combined internal+external hex
     intflash.elf - Internal flash, elf debug
     intflash.hex - Internal flash, hex
     -------------------------------------------------------------------
     STM32CubeProgrammer v2.18.0 
     -------------------------------------------------------------------
     
     Error: No debug probe detected.
     PATHTOTHEPROJECT/MyApplication/gcc/include/flash_sections_int_ext.mk:10: recipe for target '_intflash_' failed
     make[2]: *** [_intflash_] Error 1
     makefile_boot:45: recipe for target 'flash' failed
     make[1]: *** [flash] Error 2
     ../../gcc/Makefile:8: recipe for target 'flash' failed
     make: *** [flash] Error 2
     Failed
     Failed

     

    Regards, 

    Gaetan GodartSoftware engineer at ST (TouchGFX)
    ferro
    ferroAuthor
    Lead
    Mar 5, 2025 10:50 AM UTC

    Thanks @GaetanGodart 

    "you can simply click the Program and Run Target button"

    I do not have a board, I run Simulation only. 'Program Run' is therefore not avaialable.

    ferro_0-1741171272338.png

    ferro_2-1741171391549.png

     

    "simply click the Program and Run Target button (bottom right) and not connect your board"

    I think this is not user friendly - all I want to do is build application.exe, see if it links. Not interested in running simulation not flashing.

    I'll accept your answer, please reconsider. Thanks.

     

    GaetanGodart
    ST Employee
    Mar 5, 2025 4:13 PM UTC

    It makes sense that we are not allowed to compile if we don't know the target because to compile we need the know the hardware family to get the right generated files (TouchGFXGeneratedSTM32H7xx.hpp and things like that).

    I understand that you want to see if your code (in GUI folder) will compile.
    To do so, you can create your project on a TBS to be able to compile.
    When you want to go back to a simulator (or choose another TBS, perhaps one that you made), you can just create your new project and go to Edit => Import => GUI and select the project you created.

     

    Regards,

    Gaetan GodartSoftware engineer at ST (TouchGFX)
    GaetanGodart
    ST Employee
    Mar 7, 2025 12:08 PM UTC

    Hello @ferro ,

     

    Ok, so at the beginning I thought you wanted to compile and build the full application but you seem to only care about the GUI part since you are fine with just building the simulator part.

    So your request would be to have a button to do the same thing as the Run simulator button but stopping after the linking.
    I don't think this request would have a positive answer because there is a quick workaround that is to just run the simulator and then close the simulator. This way you will compile and link as you want but you will also have to wait a few seconds to finish the simulator build and for it to start. The drawback of this method (waiting a few seconds) to achieve the same result is probably not enough for me to push a new button.

    I am sorry I cannot give you a positive answer on that.

     

    Regards,

    Gaetan GodartSoftware engineer at ST (TouchGFX)
    ferro
    ferroAuthor
    Lead
    Mar 7, 2025 2:43 PM UTC

    "you seem to only care about [...] building the simulator part"

    Correct.

     

    "[...] probably not enough for me to push a new button"

    No button needed. I never use them - too much effort to move the mouse. Always F-keys, always. Mapping F3 (or Ctrl+B) to "stop after link" feature would be good enough.

     

    "I am sorry I cannot give you a positive answer on that."

    No problem at all @GaetanGodart , thanks for considering.

    unsigned_char_array
    Lead III
    Mar 7, 2025 3:01 PM UTC

    You can build the project in Visual Studio. The benefit is that you can also debug the project.

    "Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."