Skip to main content
Vojtěch
Associate
Dec 19, 2022 11:44 AM UTC
Question

GFX designer invalid patch STM32F7 disco

Hello,

I created a project in Touch GFX designer. Then I open in STM32cubeIDE, but I get a warning:

Description   Resource   Path   Location   Type

Invalid project path: Include path not found (C:\TouchGFXProjects\MyApplication_1\Middlewares\Third_Party\FreeRTOS\Source\CMSIS_RTOS).   STM32F746G_DISCO      pathentry   Path Entry Problem

thank you for answer

This topic has been closed for replies.

6 replies

Yoann KLEIN
ST Employee
Dec 19, 2022 12:39 PM UTC

Hello @Vojt?ch​ ,

Did you enable FreeRTOS in CubeMX and generated code ?

/Yoann

Yoann KLEINST Software Developer | TouchGFX
Vojtěch
VojtěchAuthor
Associate
Dec 19, 2022 12:55 PM UTC

My project was generated by Touch gfx designer. Then I ran the code in stm32cubeIDE.

Yoann KLEIN
ST Employee
Dec 19, 2022 1:05 PM UTC

I cannot reproduce your error, which version of TouchGFX are you using ?

Yoann KLEINST Software Developer | TouchGFX
Vojtěch
VojtěchAuthor
Associate
Dec 19, 2022 1:07 PM UTC

Touch GFX 4.20.0

Yoann KLEIN
ST Employee
Dec 19, 2022 1:10 PM UTC

Could you please generate code in CubeMX for this project ?

Yoann KLEINST Software Developer | TouchGFX
Karl Yamashita
Super User
Dec 20, 2022 12:38 AM UTC

Somehow your path to /Third_Party/FreeRTOS/Source/CMSIS_RTOS doesn't seem right if you had TouchGFX generate the code.

When I create a project from TouchGFX, import into STM32CubeIDE and build, I see /Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source