Skip to main content
AMull.11
Associate III
February 17, 2021
Question

Getting HardFault error when Loading Touchgfx files to external flash

Hi all,

I am doing one project where TouchGFX data has to be store in External Flash.

For this I created Custom External loader for QSPI Flash.

Tested this external loader in STM32CubeProgrammer by writing and reading 1Mb of data, and its working fine.

And also TouchGFX with internal flash its working fine.

But once I added the External Loader for TouchGFX project then code is going into HardFault Error.

Also I added below script still its is going into HardFault Error.

/* Memories definition */

MEMORY

{

 DTCMRAM  (xrw)  : ORIGIN = 0x20000000,  LENGTH = 128K

 ITCMRAM  (xrw)  : ORIGIN = 0x00000000,  LENGTH = 64K

 RAM_D1  (xrw)  : ORIGIN = 0x24000000,  LENGTH = 512K

 RAM_D2  (xrw)  : ORIGIN = 0x30000000,  LENGTH = 288K

 RAM_D3  (xrw)  : ORIGIN = 0x38000000,  LENGTH = 64K

 FLASH  (rx)  : ORIGIN = 0x8000000,  LENGTH = 2048K

 QSPI   (r)  : ORIGIN = 0x90000000,  LENGTH = 32M

}

FontFlashSection :

 {

  *(FontFlashSection FontFlashSection.*)

  *(.gnu.linkonce.r.*)

  . = ALIGN(0x4);

 } >QSPI

 TextFlashSection :

 {

  *(TextFlashSection TextFlashSection.*)

  *(.gnu.linkonce.r.*)

  . = ALIGN(0x4);

 } >QSPI

 ExtFlashSection :

 {

  *(ExtFlashSection ExtFlashSection.*)

  *(.gnu.linkonce.r.*)

  . = ALIGN(0x4);

 } >QSPI

MCU = STM32H743BIT6

IDE = STM32CubeIDE (1.5.0)

Generator Tool = STM32CubeMX (6.1.0)

Graphics = TouchGFX (4.16.0)

it will be appreciated if someone explain what to do additionally.

This topic has been closed for replies.