Skip to main content
Tuoman
Senior II
February 9, 2021
Question

get current View identification from Model?

Is there any way in TouchGFX to get any identification/handle/etc. of the current View?

I have one View that is accessible everywhere, and from that I want to return to the previous View.

How can store the previous View? Is a custom variable required for this + implementation in every single Presenter to store that custom variable?

This topic has been closed for replies.

3 replies

zzzzz
Senior
February 9, 2021

You don't have to use the presenter. I had a similar problem a while ago.

At first, I created a global variable. Say "enum Previous_Screen". Set this variable before a jump to that common screen. Base on this variable value, return to the previous screen. But the screen transition function is a template. I have to use switch statements to handle screen transitions. The code became long-winded as more screens added.

In the end, I made this common view a customer container and add it where need it.

Tuoman
TuomanAuthor
Senior II
February 10, 2021

>I have to use switch statements to handle screen transitions. The code became long-winded as more screens added.

This is what I'm trying to avoid. Sorry didn't understand, did you achieve this without custom enum? I have 50 screens, such approach would be very laborious. There has to be a better way...

zzzzz
Senior
February 10, 2021

In my case, I made a custom container to replace that common screen and added it to the screens which need it.

​

Application class provides interfaces for manipulating screen contents. I didn't find anything there. I can only think of two things to track the previous screen, model, or a global variable. But both cases need a switch statement at the end.

​Maybe TGFX employees know a better way.

​

​