Skip to main content
Aarra.1
Associate III
September 30, 2021
Solved

Generating an application for STM32H757I-Eval using TouchGFX

Hello,

I'm new to TouchGFX software.

I'm trying to use the display for the STM32H757I-Eval board.

I have configured a GUI template using the TouchGFX software. Below is the procedure I followed:

Using STM32CUBEMX in the default mode and enabled the TouchGFX and specified the dimensions of the board for the STM32H757I-eval board.

Then generated the STM32 cube IDE code.

Now from STM32 cube ide I opened the TouchGFX .part file and selected the blank UI and selected some parameters and generated the code.

Next when I built the code I am receiving the following errors.

14:50:09 **** Incremental Build of configuration Debug for project DEMO_DISPLAY_CM4 ****

make -j4 all 

arm-none-eabi-g++ "../TouchGFX/target/generated/OSWrappers.cpp" -mcpu=cortex-m4 -std=gnu++14 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H757xx -c -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Core/Inc -I../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/target/generated/OSWrappers.d" -MT"TouchGFX/target/generated/OSWrappers.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/target/generated/OSWrappers.o"

arm-none-eabi-g++ "../TouchGFX/target/generated/TouchGFXConfiguration.cpp" -mcpu=cortex-m4 -std=gnu++14 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H757xx -c -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Core/Inc -I../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/target/generated/TouchGFXConfiguration.d" -MT"TouchGFX/target/generated/TouchGFXConfiguration.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/target/generated/TouchGFXConfiguration.o"

arm-none-eabi-g++ "../TouchGFX/target/generated/TouchGFXGeneratedHAL.cpp" -mcpu=cortex-m4 -std=gnu++14 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H757xx -c -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Core/Inc -I../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/target/generated/TouchGFXGeneratedHAL.d" -MT"TouchGFX/target/generated/TouchGFXGeneratedHAL.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/target/generated/TouchGFXGeneratedHAL.o"

arm-none-eabi-g++ "../TouchGFX/target/STM32TouchController.cpp" -mcpu=cortex-m4 -std=gnu++14 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H757xx -c -I../TouchGFX/App -I../TouchGFX/target/generated -I../TouchGFX/target -I../Core/Inc -I../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"TouchGFX/target/STM32TouchController.d" -MT"TouchGFX/target/STM32TouchController.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "TouchGFX/target/STM32TouchController.o"

In file included from ../TouchGFX/target/STM32TouchController.cpp:20:

../TouchGFX/target/STM32TouchController.hpp:23:10: fatal error: platform/driver/touch/TouchController.hpp: No such file or directory

  23 | #include <platform/driver/touch/TouchController.hpp>

   |     ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

../TouchGFX/target/generated/TouchGFXConfiguration.cpp:17:10: fatal error: texts/TypedTextDatabase.hpp: No such file or directory

  17 | #include <texts/TypedTextDatabase.hpp>

   |     ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~

../TouchGFX/target/generated/OSWrappers.cpp:19:10: fatal error: touchgfx/hal/HAL.hpp: No such file or directory

  19 | #include <touchgfx/hal/HAL.hpp>

   |     ^~~~~~~~~~~~~~~~~~~~~~

In file included from ../TouchGFX/target/generated/TouchGFXGeneratedHAL.cpp:18:

../TouchGFX/target/generated/TouchGFXGeneratedHAL.hpp:20:10: fatal error: touchgfx/hal/HAL.hpp: No such file or directory

  20 | #include <touchgfx/hal/HAL.hpp>

   |     ^~~~~~~~~~~~~~~~~~~~~~

compilation terminated.

compilation terminated.

compilation terminated.

compilation terminated.

make: *** [TouchGFX/target/generated/subdir.mk:25: TouchGFX/target/generated/TouchGFXGeneratedHAL.o] Error 1

make: *** Waiting for unfinished jobs....

make: *** [TouchGFX/target/generated/subdir.mk:25: TouchGFX/target/generated/OSWrappers.o] Error 1

make: *** [TouchGFX/target/subdir.mk:25: TouchGFX/target/STM32TouchController.o] Error 1

make: *** [TouchGFX/target/generated/subdir.mk:25: TouchGFX/target/generated/TouchGFXConfiguration.o] Error 1

"make -j4 all" terminated with exit code 2. Build might be incomplete.

I am aware of the fact that TouchGFX does not generate the cube ide and cube mx files for the STM32H747I-eval ...... or does it?

Whereas I can see that all the files have been included successfully in the directory.

Please provide a solution on how can I create a project using touchGFX for STM32H757i-eval board.

Or if there is any other softwares that I can use for the same.

Hoping for a reply soon.

Regards

This topic has been closed for replies.
Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
September 30, 2021

Hi,

What is your display interface ? Are you using the display given with the board or a custom one ? As you can see from the error message it cannot find TouchController.cpp or other files , so maybe have a look at the library path settings in STM32CubeIDE. I am still not that used to dual cores so it might be a bit annoying .

Concerning the STM32H747-eval the current version of the TBS is not based on STM32CubeMX. There are also no STM32CubeIDE project associated. A new version of the TBS should hopefully come out in the coming month. Meanwhile the TBS for the STM32H747-disco does contain a STM32CubeMX and STM32CubeIDE project so you can use it as source of inspiration to configure your board for now as they are using the same display (to double check I may be wrong).

/Romain

4 replies

Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
September 30, 2021

Hi,

What is your display interface ? Are you using the display given with the board or a custom one ? As you can see from the error message it cannot find TouchController.cpp or other files , so maybe have a look at the library path settings in STM32CubeIDE. I am still not that used to dual cores so it might be a bit annoying .

Concerning the STM32H747-eval the current version of the TBS is not based on STM32CubeMX. There are also no STM32CubeIDE project associated. A new version of the TBS should hopefully come out in the coming month. Meanwhile the TBS for the STM32H747-disco does contain a STM32CubeMX and STM32CubeIDE project so you can use it as source of inspiration to configure your board for now as they are using the same display (to double check I may be wrong).

/Romain

Aarra.1
Aarra.1Author
Associate III
September 30, 2021

Hello sir,

Thank you for the quick response.

I'm using the display given with the board.

I have checked the library path settings too and all the files are included.

Thank you for your response I will surely look into this.

Regards.

MM..1
Super User
September 30, 2021

Report your versions IDE MX TGFX ...

Aarra.1
Aarra.1Author
Associate III
October 1, 2021

Hello,

Following are the software versions that I'm using.

STM32CubeIDE 1.7.0

TouchGFX 4.17.0

STM32CubemX 6.3.0

Regards.