Skip to main content
Vins
Associate III
Mar 22, 2022 11:24 AM UTC
Solved

Generated project from Cube MX with Touch GFX is generating the errors.

Hi Community,

When I generate the touch gfx combined project using cubemx I am getting the following errors.

Even though I gave the path, but still the errors exists.

../TouchGFX/target/generated/TouchGFXConfiguration.cpp:18:10: fatal error: texts/TypedTextDatabase.hpp: No such file or directory.

 

../TouchGFX/target/generated/TouchGFXGeneratedHAL.hpp:21:10: fatal error: touchgfx/hal/HAL.hpp: No such file or directory.

 

../TouchGFX/target/STM32TouchController.hpp:24:10: fatal error: platform/driver/touch/TouchController.hpp: No such file or directory.

 

../TouchGFX/target/generated/OSWrappers.cpp:20:10: fatal error: touchgfx/hal/HAL.hpp: No such file or directory.

 

../TouchGFX/target/generated/TouchGFXGeneratedHAL.hpp:21:10: fatal error: touchgfx/hal/HAL.hpp: No such file or directory.

Any suggestions to solve this would be greatly appreciated!

Thank you.

Vins.

This topic has been closed for replies.
Vins
VinsBest answer
Associate III
Aug 10, 2022 5:15 AM UTC

Hi @RLarr.1​ 

Follow the steps.

Step 1: Create a New STM32CubeIDE Project

1) In STM32CubeIDE > File > New > Select Part Number > Next > Set ProjectName > Click Finish

2) Enable SYS > Serial Wire (other configs can be made later)

3) Save and close ProjectName.IOC

4) Build Project (Compiling should be successful!)

Step 2: Add TouchGFX 4.20.0 to the Project

5) Open ProjectName.IOC > Enable CRC > Software Packs > Select Component > TouchGFX 4.20.0

6) Expand Software Packs > Enable Graphic Application > *LEAVE ALL TouchGFX SETTINGS TO DEFAULT*

7) Save and close IOC *DO NOT BUILD THE PROJECT *

Step 3: Generate TouchGFX 4.20.0 Templates

8) Double-click on \TouchGFX\ApplicationTemplate.touchgfx.part

9) Select "Blank UI" > Click red Import button > Click Generate Code > Close Designer using the X

Step 4: Clean & Compile Project

10) Right-click ProjectName > Select "Clean Project"

11) Right-click ProjectName > Select "Build Project" (Compiling should be successful at this stage!)

Step 5: ToughGFX Configurations and Code generation

12) Open ProjectName.IOC > Software Packs > TouchGFX > Set Screen Resolution e.g. 240x240, etc

13) Double-click on \TouchGFX\ApplicationTemplate.touchgfx.part, Click Generate Code > Close Designer using the X

14) Right-click ProjectName > Select "Clean Project"

15) Right-click ProjectName > Select "Build Project" (Compiling should be successful at this stage!)

/Vins

5 replies

Vins
VinsAuthor
Associate III
Mar 23, 2022 12:43 PM UTC

Hello @Martin KJELDSEN​ ,

CubeIDE - 1.9.0 and TouchGFX 4.19.0 integration issues are not yet solved. Still I am getting the errors. I saw your video https://youtu.be/VOs2LYO7wSA and tried, but issues are not yet solved. So, any other way to solve these errors?

(I am using STM32F769AIY6TR).

RLarr.1
Associate III
Aug 9, 2022 4:58 PM UTC

I am getting the same errors now 5 months from the original post. My project is a new from scratch after updating all three tools.

STM32CubeIDE Version: 1.10.1 Build: 12716_20220707_0928 (UTC)

STM32CubeIDE Version: 1.10.1 Build: 12716_20220707_0928 (UTC)

TouchGFX Version 4.20.0

Any help or guidance would be appreciated.

RLarr.1
Associate III
Aug 9, 2022 7:24 PM UTC

If I right click on the #include <platform/driver/touch/TouchController.hpp> and select Open Declaration the file opens in STM32CubeIDE but still has the red X to the left saying no such file or directory and fails to build.

Vins
VinsAuthorBest answer
Associate III
Aug 10, 2022 5:15 AM UTC

Hi @RLarr.1​ 

Follow the steps.

Step 1: Create a New STM32CubeIDE Project

1) In STM32CubeIDE > File > New > Select Part Number > Next > Set ProjectName > Click Finish

2) Enable SYS > Serial Wire (other configs can be made later)

3) Save and close ProjectName.IOC

4) Build Project (Compiling should be successful!)

Step 2: Add TouchGFX 4.20.0 to the Project

5) Open ProjectName.IOC > Enable CRC > Software Packs > Select Component > TouchGFX 4.20.0

6) Expand Software Packs > Enable Graphic Application > *LEAVE ALL TouchGFX SETTINGS TO DEFAULT*

7) Save and close IOC *DO NOT BUILD THE PROJECT *

Step 3: Generate TouchGFX 4.20.0 Templates

8) Double-click on \TouchGFX\ApplicationTemplate.touchgfx.part

9) Select "Blank UI" > Click red Import button > Click Generate Code > Close Designer using the X

Step 4: Clean & Compile Project

10) Right-click ProjectName > Select "Clean Project"

11) Right-click ProjectName > Select "Build Project" (Compiling should be successful at this stage!)

Step 5: ToughGFX Configurations and Code generation

12) Open ProjectName.IOC > Software Packs > TouchGFX > Set Screen Resolution e.g. 240x240, etc

13) Double-click on \TouchGFX\ApplicationTemplate.touchgfx.part, Click Generate Code > Close Designer using the X

14) Right-click ProjectName > Select "Clean Project"

15) Right-click ProjectName > Select "Build Project" (Compiling should be successful at this stage!)

/Vins