Skip to main content
AWack
Associate III
Nov 19, 2024 1:40 PM UTC
Solved

General concept for non-GUI user code in TouchGFX

Hi,

I´ve to start a project (with FreeRTOS) where several code has to be implemented which is not directly related to the GUI (some state machines, control algorithms, ...).

I´m not sure, if I should implement this code parts as usual in my FreeRTOS and exchange only GUI data with the model, or if I should implement also my non GUI related code in the model?

 

Best regards,

Achim

This topic has been closed for replies.
GaetanGodart
GaetanGodartBest answer
ST Employee
Nov 19, 2024 3:29 PM UTC

Hello @AWack ,

 

Both would work.
You could include your main.h in the model.cpp to have access to the variables that are changed in main.c, this is straight forward and better for simple applications.
You could also use the RTOS if you have one which is great if you would need the semaphores / queue / other features of the RTOS so it is more suited for more complex applications.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)

2 replies

GaetanGodart
GaetanGodartBest answer
ST Employee
Nov 19, 2024 3:29 PM UTC

Hello @AWack ,

 

Both would work.
You could include your main.h in the model.cpp to have access to the variables that are changed in main.c, this is straight forward and better for simple applications.
You could also use the RTOS if you have one which is great if you would need the semaphores / queue / other features of the RTOS so it is more suited for more complex applications.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
GaetanGodart
ST Employee
Dec 10, 2024 2:07 PM UTC

Hello @AWack ,

 

Have you been able to move forward with your issue?
If you did, could you select the comment that helped you the most as "best answer".

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)