Associate II
Jul 25, 2016 3:06 PM UTC
Question
FSMC generating an extra write cycle
- 8 replies
- 2150 views
Posted on July 25, 2016 at 17:06
I've developed code to drive an SSD1305 graphical LCD controller over an 8 bit parallel bus both via the FSMC & for comparison, bit banged. The FSMC generates 2 chip select pulses, but only puts data on the bus for the first one.
I'm using the peripheral libraries on an F407. I've attached the FSMC setup code. I'll attach some scope traces next... Regards Ken #fsmc #scope-traces-f407-lcd-tft #scope-traces-f407-lcd-tft