Skip to main content
JB91
Associate
Sep 18, 2019 6:28 AM UTC
Solved

Framebuffer splitting in internal RAM

Im working on a STM32F407 MCU with an 320x240 px Display (16bit colors) connected to the FSMC. Id like to avoid using an external RAM.

Is it possible to have a smaller Framebuffer located in the internal RAM?

I guess it could be interesting to vary the buffer size to for example to 40 lines ( 320x40x16bit in my example) and putting the area to the internal RAM.

If its not possible might it be interesting to make a feature request?

Thank you in advance.

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
Sep 18, 2019 10:40 AM UTC

Not concretely. Internal deadlines are preventing us from releasing new versions, but this is being mitigated. Soon we'll have no restrictions on releasing new versions.

Hope that's enough of an answer!

/Martin

5 replies

Martin KJELDSEN
Principal III
Sep 18, 2019 6:56 AM UTC

Hi @JB91​,

Of course =) Just provide touchgfx with an address in internal memory instead of pointing to external RAM. Here's an example for how to configure touchgfx to use a single framebuffer in internal ram (most often, fitting two framebuffers in internal RAM is not feasible).

uint16_t frameBuffer[480 * 272];
static uint16_t frameBuf0 =&frameBuffer[0];
...
hal.setFrameBufferStartAddress((uint16_t*)frameBuf0, 16);

/Martin

JB91
JB91Author
Associate
Sep 18, 2019 8:52 AM UTC

Hi @Martin KJELDSEN​ ,

thanks for your quick answer.

Is it also possible to raster the framebuffer in order reduce the size of the framebuffer?

**example:**

  • Display with ILI9341 controller, 320px * 240px and 16bit color depth needs 154kByte for a full single framebuffer

With rastering it could be possible to split the framebuffer into several parts.

  • using only 40 lines for the temporary framebuffer would need 320px * 40px = 25kByte RAM
  • the parts are then processed sequentially
Martin KJELDSEN
Principal III
Sep 18, 2019 9:14 AM UTC

Hi @JB91​,

In newer, yet to be released verisons of touchgfx, we support 8-bit palette and also partial framebuffers which both lower the overall memory requirements.

/Martin

JB91
JB91Author
Associate
Sep 18, 2019 9:55 AM UTC

Hi @Martin KJELDSEN​ ,

do you know when the new version will be released?

Thanks,

Josh

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
Sep 18, 2019 10:40 AM UTC

Not concretely. Internal deadlines are preventing us from releasing new versions, but this is being mitigated. Soon we'll have no restrictions on releasing new versions.

Hope that's enough of an answer!

/Martin