Skip to main content
CarlsbadJerry
Associate II
May 5, 2021 5:01 PM UTC
Solved

For the STM32L476 Discovery board, if I remove the LCD, can I use the now free pins on the two connectors for alternate purposes, or do I need any other electrical configuration?

Basically, I'm hoping to try out a different Microphone on SAI_2 and it looks like those pins would be freed up by removing the LCD display.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 5, 2021 6:05 PM UTC

The schematic would be the controlling document as to whether pins are cross connected, or to other parts/circuits on the board.

But generally yes, removing the LCD will significantly reduces the conflicts, and then you'd need to remove any code in the BSP/MSP files within a project or which would otherwise try to initialize/use the pins for the LCD use case in the examples.

The pins can then be used for GPIO, or other Alternate Functions as described in the Data Sheet.

The L4 provided for pin-level muxing of functionality, so the option should be fairly broad.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 5, 2021 6:05 PM UTC

The schematic would be the controlling document as to whether pins are cross connected, or to other parts/circuits on the board.

But generally yes, removing the LCD will significantly reduces the conflicts, and then you'd need to remove any code in the BSP/MSP files within a project or which would otherwise try to initialize/use the pins for the LCD use case in the examples.

The pins can then be used for GPIO, or other Alternate Functions as described in the Data Sheet.

The L4 provided for pin-level muxing of functionality, so the option should be fairly broad.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
CarlsbadJerry
Associate II
May 5, 2021 9:17 PM UTC

Thanks! I appreciate your quick answer. I'll look at the schematic once more, but I believe it should work.

Cheers, Jerry