Skip to main content
JKhal
Associate III
February 18, 2020
Question

FMC and Code Generation Issue

Hi,

I am developing an application running on STM32F469 MCU to control an LCD

Generating my Code using STM32CubeMX.

Using FMC Memry type is LCD_Interface, A23 Data: 16 bits

The bug I found is in the STemwin_wrapper.c file, in functions : FMC_BANK_WriteData and FMC_BANK_ReadData.

the bug is that the code generated tries to write and read the data from  FMC_BANK->RAM and that address is 0x60000002 where it have to be 0x61000000

typedef struct
 
{
 __IO uint16_t REG;
 __IO uint16_t RAM;
 
}LCD_CONTROLLER_TypeDef;
 
/* The Bank address need to be entred by the USER */
#define FMC_BANK_BASE ((uint32_t) 0x60000000 )
#define FMC_BANK ((LCD_CONTROLLER_TypeDef *) FMC_BANK_BASE)
 
/**
 * @brief Writes register value.
 * @param Data: 
 * @retval None
 */
static void FMC_BANK_WriteData(uint16_t Data) 
{
 /* Write 16-bit Reg */
 *(uint16_t*)0x61000000 = Data; // FMC_BANK->RAM = Data;
}
 
/**
 * @brief Writes register address.
 * @param Reg: 
 * @retval None
 */
static void FMC_BANK_WriteReg(uint8_t Reg) 
{
 /* Write 16-bit Index, then write register */
 FMC_BANK->REG = Reg;
}
 
/**
 * @brief Reads register value.
 * @param None
 * @retval Read value
 */
static uint16_t FMC_BANK_ReadData(void) 
{
 return *(uint16_t*)0x61000000 ; // return FMC_BANK->RAM;
}
 
 

the issue is that every time I regenerate the code using STM32CubeMX the bug returns and have to fix it again.

is there a way to avoid this bug regenerating or better to fix it from the beginning?

This topic has been closed for replies.

1 reply

Nesrine.JLASSI
Visitor II
April 21, 2020

Hello @Community member​ 

Could you please share your .ioc to check the issue .

Best regards,

Nesrine