Skip to main content
Associate
Jul 9, 2025 10:45 AM UTC
Question

Flickering in middle of 7-inch LTDC display

Hello,

I am using the STM32H743IITG microcontroller with a 7-inch RGB888 interface display. I have integrated TouchGFX using STM32CubeIDE.

The problem is that I am seeing flickering in the middle of the display. This flickering occurs when I add a box widget in TouchGFX.

Has anyone faced a similar issue or can suggest how to resolve it?

Thanks in advance!

checkkkk.jpeg

 

This topic has been closed for replies.

6 replies

jumman_JHINGA
Senior III
Jul 9, 2025 11:20 AM UTC

There would be many reasons like, LTDC parameters, LTDC Frequency, FrameBuffer Size (Single Double), SDRAM Configurations (Speed, Timings, etc), if your using QuadSPI ( speed, memory mapped). 

or could be a hardware issue like Loos FPC connection, Track lenght etc.

you need to debug these things first. 

Associate
Jul 11, 2025 10:02 AM UTC

hello sir when iam drawing the solid colour to the display iam getting the same colour on display but when iam trying to draw any shapes on the display then iam getting the distortion 

 sir iam using the ltdc 24 bit ARG888 and my ltdc configuration are show in bellow 

and my ltdc clock is 26.6 Mhz

hltdc.Instance = LTDC;

hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL;

hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL;

hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AL;

hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC;

hltdc.Init.HorizontalSync = 47;

hltdc.Init.VerticalSync = 2;

hltdc.Init.AccumulatedHBP = 87;

hltdc.Init.AccumulatedVBP = 34;

hltdc.Init.AccumulatedActiveW = 975;

hltdc.Init.AccumulatedActiveH = 514;

hltdc.Init.TotalWidth = 1015;

hltdc.Init.TotalHeigh = 527;

hltdc.Init.Backcolor.Blue = 0;

hltdc.Init.Backcolor.Green = 0;

hltdc.Init.Backcolor.Red = 0;

if (HAL_LTDC_Init(&hltdc) != HAL_OK)

{

Error_Handler();

}

pLayerCfg.WindowX0 = 0;

pLayerCfg.WindowX1 = 800;

pLayerCfg.WindowY0 = 0;

pLayerCfg.WindowY1 = 480;

pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_ARGB8888;

pLayerCfg.Alpha = 255;

pLayerCfg.Alpha0 = 0;

pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_CA;

pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_CA;

pLayerCfg.FBStartAdress = 0xD0000000 ;

pLayerCfg.ImageWidth = 800;

pLayerCfg.ImageHeight = 480;

pLayerCfg.Backcolor.Blue = 0;

pLayerCfg.Backcolor.Green = 0;

pLayerCfg.Backcolor.Red = 255;

if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK)

{

Error_Handler();

}

And one more thing when i changeing the ARGB888 to RGB888 format then iam drawing any shape iam

getting the shape on the display but the colous is not pure(some stipes between the colour) please see the below picture.

 

 

test_touch.jpeg

 

ididnt understand the problem sir and one more thing iam using the external sdram and my configurations

is

 
static void MX_FMC_Init(void)

{



/* USER CODE BEGIN FMC_Init 0 */



/* USER CODE END FMC_Init 0 */



FMC_SDRAM_TimingTypeDef SdramTiming = {0};



/* USER CODE BEGIN FMC_Init 1 */



/* USER CODE END FMC_Init 1 */



/** Perform the SDRAM1 memory initialization sequence

*/

hsdram1.Instance = FMC_SDRAM_DEVICE;

/* hsdram1.Init */

hsdram1.Init.SDBank = FMC_SDRAM_BANK2;

hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_8;

hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12;

hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_32;//FMC_SDRAM_MEM_BUS_WIDTH_16;

hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;

hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3;

hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;

hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2;

hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_DISABLE;

hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_0;

/* SdramTiming */

SdramTiming.LoadToActiveDelay = 2;

SdramTiming.ExitSelfRefreshDelay = 7;

SdramTiming.SelfRefreshTime = 4;

SdramTiming.RowCycleDelay = 6;

SdramTiming.WriteRecoveryTime = 2;

SdramTiming.RPDelay = 2;

SdramTiming.RCDDelay = 2;



if (HAL_SDRAM_Init(&hsdram1, &SdramTiming) != HAL_OK)

{

Error_Handler( );

}



/* USER CODE BEGIN FMC_Init 2 */



/* USER CODE END FMC_Init 2 */

}

FMC_SDRAM_CommandTypeDef Command;

__IO uint32_t tmpmrd = 0;



/* Step 1: Configure a clock configuration enable command */

Command.CommandMode = FMC_SDRAM_CMD_CLK_ENABLE;

Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;

Command.AutoRefreshNumber = 1;

Command.ModeRegisterDefinition = 0;



HAL_SDRAM_SendCommand(&hsdram1, &Command, HAL_MAX_DELAY);



/* Step 2: Insert 100 ms delay */

HAL_Delay(100);



/* Step 3: Configure a PALL (precharge all) command */

Command.CommandMode = FMC_SDRAM_CMD_PALL;

HAL_SDRAM_SendCommand(&hsdram1, &Command, HAL_MAX_DELAY);



/* Step 4: Configure an Auto Refresh command */

Command.CommandMode = FMC_SDRAM_CMD_AUTOREFRESH_MODE;

Command.AutoRefreshNumber = 8;

HAL_SDRAM_SendCommand(&hsdram1, &Command, HAL_MAX_DELAY);



/* Step 5: Configure the external memory mode register */

tmpmrd = (uint32_t) SDRAM_MODEREG_BURST_LENGTH_1 |

SDRAM_MODEREG_BURST_TYPE_SEQUENTIAL |

SDRAM_MODEREG_CAS_LATENCY_3 |

SDRAM_MODEREG_OPERATING_MODE_STANDARD |

SDRAM_MODEREG_WRITEBURST_MODE_SINGLE;



Command.CommandMode = FMC_SDRAM_CMD_LOAD_MODE;

Command.ModeRegisterDefinition = tmpmrd;



HAL_SDRAM_SendCommand(&hsdram1, &Command, HAL_MAX_DELAY);



/* Step 6: Set the refresh rate */

HAL_SDRAM_ProgramRefreshRate(&hsdram1, 683); // For 64ms / 8192 rows ≈ 7.8 µs per refresh

and these datasheet are uploaded below


Edited to apply source code formatting - please see How to insert source code for future reference.

jumman_JHINGA
Senior III
Jul 12, 2025 4:53 AM UTC

Are you using DMA2D and Chrome ART accelarator?

 

Associate
Jul 14, 2025 4:04 AM UTC

No sir iam not using the DMA2D and Chrome ART accelarator

jumman_JHINGA
Senior III
Jul 14, 2025 4:38 AM UTC

then, try DMA2D and Chrome ART accelarator. this might resolve your issue

Associate
Jul 16, 2025 6:58 AM UTC

I will try and update to you sir