Skip to main content
unsigned_char_array
Lead III
Sep 27, 2024 2:32 PM UTC
Question

Feature request: smaller generated image source files (e.g. image_EXAMPLE_IMAGE.cpp)

Currently image source files take up a lot of drive space.

My image folder TouchGFX\generated\images\src is 44.5MiB on my drive.

TouchGFX projects can take up a lot of drive space as is (https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/gfxdesigner-option-to-auto-delete-touchgfx-folder-upon-exit/m-p/724758#M39655). So these files just add to it.

You could use build scripts or cmake to add data from binary files to temporary source files. But this can be quite a hassle to make it platform independent. But that would save a lot of drive space as the binary files take up less space than source files with hex constants. (Example to use OBJCOPY)

There are ways to shrink the source files. One way is to use uint64_t hex constants instead of uint8_t hex constants to reduce overhead.
Before:

 

 

LOCATION_PRAGMA("ExtFlashSection")
KEEP extern const unsigned char image_test_image[] LOCATION_ATTRIBUTE("ExtFlashSection") = { // a x b RGB565 pixels.
0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0A, 0x0B, 
0x0C, 0x0D, 0x0E, 0x0F, 0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17, 
0x18, 0x19, 0x1A, 0x1B, 0x1C, 0x1D, 0x1E, 0x1F, ...
};

 

After:

header file:

 

template <typename... T>
constexpr std::array<uint8_t, sizeof...(T)*8> u64_array_to_u8_array(T&&... t) 
{
 std::array<uint8_t, sizeof...(T)*8> out{};
 std::array<int64_t, sizeof...(T)> in = {t...};

 for (size_t i = 0; i < sizeof...(T)*8; ++ i) {
 out[i] = uint64_t(in[i/8]) >> ((7-i%8)*8);//big endian
 }
 return out;
}

 

smaller source file:

 

LOCATION_PRAGMA("ExtFlashSection")
KEEP extern const unsigned char image_test_image[] LOCATION_ATTRIBUTE("ExtFlashSection") = // a x b RGB565 pixels.
u64_array_to_u8_array(
 0x0001020304050607,0x08090A0B0C0D0E0F,
 0x1011121314151617,0x18191A1B1C1D1E1F, ...
);

 

Large files can easily be 50% smaller on drives this way. Especially with wider lines and without whitespace.
I don't know how this affects compression of source files.

Using base64 would work too, but that would require c++17 or c++20 and by default TouchGFX uses c++14. Also it won't compress as well in zip or in git. Here is an example of base64: https://stackoverflow.com/a/79042473/15307950

 

    16 replies

    Andrew Neil
    Super User
    Sep 27, 2024 2:42 PM UTC

    Now I remember the days when 20MiB was a good size for a hard drive but, with Tera-byte drives being commonplace nowadays - is this really an issue?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    unsigned_char_array
    Lead III
    Sep 27, 2024 2:59 PM UTC

    Without trimming some files and removing build artifacts a TouchGFX project folder easily gets to be 1GiB. I find that a lot for embedded software source code. My folder for TouchGFX projects is more than 10GiB. That's still significant for disk space. All these projects are also stored in version control and also backed up so every byte counts multiple times.
    I keep several versions of TouchGFX installed and each of them is about 1.5GiB too. STM32CubeIDE is 3GiB.
    For my work PC it is not a problem, but my home PC runs out of disk space quite easily.

    This may not seem like a lot, but combined with other methods (removing unused files, see other topic I linked in my post) I think this can save many users a lot of disk space and I think it is worth at least considering.

    "Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
    Tesla DeLorean
    Guru
    Sep 27, 2024 4:24 PM UTC

    Ok, but how much of the 10GB is clag generated at compile time?

    One of the problems with bit maps is holding them in original and intermediate forms, perhaps multiple.

    Having them as C arrays makes for compatibility and compilability, but not for image editing.

    The linker should be able to pull binary data, other platforms allow for binaries to be included directly via assembler or linker directives, but this is highly non-portable.

    Lot of choices and options, most unlikely to be desirable to the entire audience.

    Editing tools (image) that can natively import/export in a C source form would reduce a number of headaches and necessity to hold multiple forms of the same data.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    Sep 27, 2024 4:17 PM UTC

    The first example is 20% spaces

    But yes would generally agree that outputting as 32-bit words, or 64-bit double words would be more efficient, it does create some portability issues related to endianness.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    unsigned_char_array
    Lead III
    Sep 27, 2024 4:20 PM UTC

    @Tesla DeLorean wrote:

    it does create some portability issues related to endianness.


    I use shifting so there is no assumption made about endianness and it will always work. But simply using a uint64_t array would also work as long as it matches the endianness of the platform.

    "Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
    ST Employee
    Oct 1, 2024 12:50 PM UTC

    Hello @unsigned_char_array ,

    Thanks a lot for your input. It is a valid one, and I would share it with the rest of the team to consider it for future releases, but I cannot guaranty when it will be implemented.

    Best regards,

    Mohammad MORADIST Software Developer | TouchGFX
    unsigned_char_array
    Lead III
    Jan 22, 2025 2:31 PM UTC

    Today I noted another issue with these large source files: Firmware packs are much much larger!
    Example:

    STM32Cube_FW_H7_V1.11.2
    zipped size: 1.03 GiB
    unzipped size: 3.75 GiB
    of which generated image source files from examples: 1.1GiB
    total size of STM32Cube\Repository folder with all packs: 40.4GiB

    As you can see packs take up a lot of space and a significant portion of this is generated image source files.
    It will save time on downloading and unzipping packs and will save drive space if generated image source files are stored more efficiently.

     

     

    "Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
    unsigned_char_array
    Lead III
    Jun 25, 2026 12:01 PM UTC

    Any update?

    I’m planning to create my own post-build script that shrinks these image source files on disk.

    "Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
    Osman SOYKURT
    ST Technical Moderator
    Jul 1, 2026 1:53 PM UTC

    Hello ​@unsigned_char_array ,

    I discussed this with the team today, and unfortunately it is not something we plan to address in the near future. However, if it becomes a recurring issue, I will make sure to bring it back to the team’s attention.

    ST Software Developer | TouchGFX