[Feature Request] Implement Background Widget so the Slide transition only slides the other widgets but not the background.
Pretty advanced feature I'm requesting here, but would it be possible to have a Background Widget so it can be excluded from the Slide screen transitions? This way, if we have an application with multiple screens that all have the same background image, we could have a Slide transition that leaves the background intact but only slides the widgets that are over the background.
I have no idea if this is even possible with the current transition implementation of Touch GFX, but it would surely make an awesome feature!
Thank you,