Skip to main content
unsigned_char_array
Lead III
Mar 27, 2025 1:18 PM UTC
Question

Feature request: Ability to hide blue border in editor

Currently the blue border masks the pixels on the edge so you cannot see what you are doing.
Example:

unsigned_char_array_0-1743081297640.png

I want to be able to select and edit the widget while also seeing it completely.
I also want to be able to zoom in more than 500% and the ability to see a pixel grid. It's easy to be off by one.

(edit: removed section about scaling of the simulator window. Moved it to this topic: https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/feature-request-integer-scaling-for-simulator-rendering/m-p/788659#M42727)

    This topic has been closed for replies.

    4 replies

    GaetanGodart
    ST Employee
    Mar 27, 2025 2:41 PM UTC

    Hello @unsigned_char_array ,

     

    Thank you for your feedback, I will inform the team about your request.

     

    Regards,

    Gaetan GodartSoftware engineer at ST (TouchGFX)
    unsigned_char_array
    Lead III
    Mar 27, 2025 4:20 PM UTC
    "Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
    ferro
    Lead
    Mar 27, 2025 5:22 PM UTC

    very interesting, thanks

    GaetanGodart
    ST Employee
    Apr 4, 2025 8:20 AM UTC

    Hello @unsigned_char_array ,

     

    We will consider improving the selection for a future release.

     

    Regards,

    Gaetan GodartSoftware engineer at ST (TouchGFX)