Skip to main content
Associate
Sep 29, 2025 1:08 PM UTC
Question

Ethernet and LWIP causing Host unreachable; fix Memory map for STM32F746 Discovery?

Currently I am struck with Ethernet communication where I am not able to communicate properly.
I have working functionality with static IP. I have implemented functionality to either enable DHCP or Static. Independently both works. When I am trying to call an event to enable DHCP or static my board hangs or freezes. Sometimes I jump into Hardfault_handler error.
 
After debugging I noticed that my memory mapping somehow I am not able to figure out the exact root cause. I am using Touchgfx as an output interface.
 
I followed your F7 videos and tried to fix the solution but didn't work. Maybe I thought of asking for your help. I share my linker script and MPU_config and also Ethernet descriptor.
 
My current script expects to keep assets text, font, extflash related to touchgfx in QSPI memory, SDRAM wants to add Touchgfx_scrollbars etc. I tried to use the QSPI location but failed. RAM memory location where I am currently facing an issue. I attached my linker script for reference. 
 
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};

/* Disable the MPU */
HAL_MPU_Disable();

/* Region 0: Internal RAM (320KB) - Non-cacheable for DMA */
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0x20000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_256KB; /* First 256KB */
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; /* For DMA */
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; /* Non-cacheable for DMA */
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);

/* Region 1: Remaining Internal RAM (64KB) */
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.BaseAddress = 0x20040000;
MPU_InitStruct.Size = MPU_REGION_SIZE_64KB;
HAL_MPU_ConfigRegion(&MPU_InitStruct);



/* Region 2: Internal FLASH (1MB) - Cacheable */
MPU_InitStruct.Number = MPU_REGION_NUMBER2;
MPU_InitStruct.BaseAddress = 0x08000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_1MB;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);

/* Region 3: QSPI Flash (16MB) - Cacheable */
MPU_InitStruct.Number = MPU_REGION_NUMBER3;
MPU_InitStruct.BaseAddress = 0x90000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_16MB;
HAL_MPU_ConfigRegion(&MPU_InitStruct);

/* Region 4: SDRAM (8MB) - Cacheable for graphics */
MPU_InitStruct.Number = MPU_REGION_NUMBER4;
MPU_InitStruct.BaseAddress = 0xC0000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_8MB;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; /* For DMA2D/LTDC */

HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enable the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
 
ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT] __attribute__((section(".RxDecripSection"), aligned(32)));
ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT] __attribute__((section(".TxDecripSection"), aligned(32)));
uint8_t Rx_Buff[ETH_RX_DESC_CNT][ETH_RX_BUF_SIZE] __attribute__((section(".RxArraySection"), aligned(32)));
uint8_t Tx_Buff[ETH_TX_DESC_CNT][ETH_TX_BUF_SIZE] __attribute__((section(".TxArraySection"), aligned(32)));
 
#define MEM_SIZE 24576
/*----- Default Value for F7 devices: 0x20048000 -----*/
#define LWIP_RAM_HEAP_POINTER 0x20048000
#define PBUF_POOL_BUFSIZE 1536 and my linker Script 
 

 

/* 
******************************************************************************
 ** @file : STM32F746NGHX_FLASH.ld
 ** @brief : Linker script for STM32F746NGHx (1024KB FLASH, 320KB RAM)
 ** - DTCM (64KB) used for stack/heap (fast, CPU-only)
 ** - AXI SRAM cached (176KB low + optional 48KB high)
 ** - ETH descriptors in SRAM2 (16KB, non-cacheable)
 ** - ETH Rx/Tx buffers in AXI 64KB non-cacheable window
 ** - TouchGFX buffers in SDRAM, assets in QSPI
 ******************************************************************************
*/

ENTRY( Reset_Handler)
/* ====== Memory map ====== */
MEMORY
{
	/* TCMs */
	ITCM_RAM (xrw) : ORIGIN = 0x00000000, LENGTH = 16K
	DTCM_RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 64K /* stack/heap, fast */
	
	/* AXI SRAM (cached regions) */
	AXI_SRAM_C (xrw) : ORIGIN = 0x20020000, LENGTH = 176K /* main .data/.bss */
	AXI_SRAM_C_HI(xrw) : ORIGIN = 0x20050000, LENGTH = 48K /* optional extras */
	
	/* AXI SRAM non-cacheable carve-outs (must match MPU) */
	ETHBUFF_NC (xrw) : ORIGIN = 0x20010000, LENGTH = 64K /* ETH Rx/Tx buffers */
	SRAM2_NC (xrw) : ORIGIN = 0x2004C000, LENGTH = 16K /* ETH descriptors */
	/* Non-volatile / external */
	FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K
	QUADSPI (r ) : ORIGIN = 0x90000000, LENGTH = 16M
	SDRAM (xrw) : ORIGIN = 0xC0000000, LENGTH = 8M
}

/* ====== Stacks & libc heap placed in DTCM ====== */
_estack = ORIGIN(DTCM_RAM) + LENGTH(DTCM_RAM);
_Min_Heap_Size = 0x0A00; /* libc heap (if used) */
_Min_Stack_Size = 0x0A00; /* process stack reserve */
/* Used by startup to copy .data from FLASH */
_sidata = LOADADDR(.data);
/* ====== Sections ====== */

SECTIONS
{
	/* Vector table in FLASH */
	.isr_vector :
	{
		. = ALIGN(4);
		KEEP(*(.isr_vector))
		. = ALIGN(4);
	}> FLASH

	/* Code */
	.text :
	{
		. = ALIGN(4);
		*(.text) *(.text*)
		*(.glue_7) *(.glue_7t)
		*(.eh_frame)
		KEEP(*(.init)) KEEP(*(.fini))
		. = ALIGN(4);
		_etext = .;
	}> FLASH

	/* Constants */
	.rodata :
	{
		. = ALIGN(4);
		*(.rodata) *(.rodata*)
		. = ALIGN(4);
	}> FLASH

	/* ARM exception tables */
	.ARM.extab (READONLY) :
	{
		. = ALIGN(4);
		*(.ARM.extab* .gnu.linkonce.armextab.*)
		. = ALIGN(4);
	}> FLASH

	.ARM (READONLY) :
	{
		. = ALIGN(4);
		__exidx_start = .;
		*(.ARM.exidx*)
		__exidx_end = .;
		. = ALIGN(4);
	}> FLASH

	.preinit_array (READONLY) :
	{
		. = ALIGN(4);
		PROVIDE_HIDDEN (__preinit_array_start = .);
		KEEP (*(.preinit_array*))
		PROVIDE_HIDDEN (__preinit_array_end = .);
		. = ALIGN(4);
	}> FLASH

	.init_array (READONLY) :
	{
		. = ALIGN(4);
		PROVIDE_HIDDEN (__init_array_start = .);
		KEEP (*(SORT(.init_array.*)))
		KEEP (*(.init_array*))
		PROVIDE_HIDDEN (__init_array_end = .);
		. = ALIGN(4);
	}> FLASH

	.fini_array (READONLY) :
	{
		. = ALIGN(4);
		PROVIDE_HIDDEN (__fini_array_start = .);
		KEEP (*(SORT(.fini_array.*)))
		KEEP (*(.fini_array*))
		PROVIDE_HIDDEN (__fini_array_end = .);
		. = ALIGN(4);
	}> FLASH

	/* --------- Initialized data in AXI cached RAM --------- */
	.data :
	{
		. = ALIGN(4);
		_sdata = .;
		*(.data) *(.data*)
		/* Optional: fast functions in RAM */
		*(.RamFunc) *(.RamFunc*)
		. = ALIGN(4);
		_edata = .;
	}> AXI_SRAM_C AT > FLASH

	/* --------- Uninitialized data in AXI cached RAM --------- */
	.bss (NOLOAD) :
	{
		. = ALIGN(4);
		_sbss = .;
		__bss_start__ = _sbss;
		*(.bss) *(.bss*) *(COMMON)
		. = ALIGN(4);
		_ebss = .;
		__bss_end__ = _ebss;
	}> AXI_SRAM_C

	/* --------- Optional high cached RAM (place large arrays manually) --------- */
	.ram_high (NOLOAD) :
	{
		. = ALIGN(4);
		*(.ram_high) *(.ram_high.*)
		. = ALIGN(4);
	}> AXI_SRAM_C_HI

	/* --------- DTCM-only data (fast, CPU-only) OPTIONAL --------- */
	.dtcm_data :
	{
		. = ALIGN(4);
		*(.dtcm_data) *(.dtcm_data.*)
		. = ALIGN(8);
	}> DTCM_RAM AT > FLASH

	.dtcm_bss (NOLOAD) :
	{
		. = ALIGN(8);
		*(.dtcm_bss) *(.dtcm_bss.*)
		. = ALIGN(8);
	}> DTCM_RAM

	/* --------- C library heap + main stack in DTCM --------- */
	._user_heap_stack :
	{
		. = ALIGN(8);
		PROVIDE(end = .);
		PROVIDE(_end = .);
		. = . + _Min_Heap_Size;
		. = . + _Min_Stack_Size;
		. = ALIGN(8);
	}> DTCM_RAM

	/* --------- Ethernet: NON-CACHEABLE --------- */
	/* Descriptors in SRAM2 (16KB) */
	.RxDecripSection (NOLOAD) :
	{
		. = ALIGN(32);
		*(.RxDecripSection) /* ETH_DMADescTypeDef Rx */
		. = ALIGN(32);
	}> SRAM2_NC

	.TxDecripSection (NOLOAD) :
	{
		. = ALIGN(32);
		*(.TxDecripSection) /* ETH_DMADescTypeDef Tx */
		. = ALIGN(32);
	}> SRAM2_NC

	/* Rx/Tx buffers in 64KB non-cacheable window */
	.ETH_NC_Buffers (NOLOAD) :
	{
		. = ALIGN(32);
		*(.ETH_NC_Buffers) /* uint8_t Rx/Tx buffers */
		. = ALIGN(32);
	}> ETHBUFF_NC

	/* --------- TouchGFX in SDRAM --------- */
	BufferSection (NOLOAD) :
	{
		. = ALIGN(64);
		*(TouchGFX_Framebuffer TouchGFX_Framebuffer.*)
		. = ALIGN(64);
	}> SDRAM

	TouchGFX_ScratchbufferA (NOLOAD) :
	{
		. = ALIGN(64);
		*(TouchGFX_ScratchbufferA TouchGFX_ScratchbufferA.*)
		. = ALIGN(64);
	}> SDRAM

	TouchGFX_ScratchbufferB (NOLOAD) :
	{
		. = ALIGN(64);
		*(TouchGFX_ScratchbufferB TouchGFX_ScratchbufferB.*)
		. = ALIGN(64);
	}> SDRAM

	/* --------- External QSPI (RO assets) --------- */
	ExtFlashSection :
	{
		. = ALIGN(4);
		*(ExtFlashSection ExtFlashSection.*)
		. = ALIGN(4);
	}> QUADSPI

	FontFlashSection :
	{
		. = ALIGN(4);
		*(FontFlashSection FontFlashSection.*)
		. = ALIGN(4);
	}> QUADSPI

	TextFlashSection :
	{
		. = ALIGN(4);
		*(TextFlashSection TextFlashSection.*)
		. = ALIGN(4);
	}> QUADSPI
	/* Discard unused standard libs */
	/DISCARD/ :
	{
		libc.a(*)
		libm.a(*)
		libgcc.a(*)
	}
	.ARM.attributes 0 : {*(.ARM.attributes)}

}
  • Call MPU_Config() before enabling caches.

  • Then SCB_EnableICache(); SCB_EnableDCache();

  • linker matches:

    • .ETH_NC_Buffers at 0x20010000 (64 KB NC)

    • .RxDecripSection/.TxDecripSection at 0x2004C000 (16 KB NC)

    • General .data/.bss in AXI cacheable (0x20020000…)

    • Stack/heap in DTCM (0x20000000…)

/* Descriptors: 32-byte aligned in SRAM2_NC */

ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT] __attribute__((section(".RxDecripSection"), aligned(32)));

ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT] __attribute__((section(".TxDecripSection"), aligned(32)));

/* Rx/Tx buffers: 32-byte aligned in AXI non-cacheable window */

uint8_t ETH_Rx_Buff[ETH_RX_DESC_CNT][ETH_RX_BUF_SIZE] __attribute__((section(".ETH_NC_Buffers"), aligned(32)));

uint8_t ETH_Tx_Buff[ETH_TX_DESC_CNT][ETH_TX_BUF_SIZE] __attribute__((section(".ETH_NC_Buffers"), aligned(32)));

please could someone guide me and correct my linker script and MPU configuration. I assume the DTCM and DMA are overlapping with the RAM memory and the buffer is not able to communicate with ARP from pc.

Looking forward for your inputs. Thank you.

@stm32f746 discovery board

This topic has been closed for replies.

3 replies

mbarg.1
Senior III
Sep 29, 2025 2:11 PM UTC

Did you check Ethernet stack size and usage ? when you enable both, you need to increase cache size.

rviswaAuthor
Associate
Sep 29, 2025 2:59 PM UTC

Hi @mbarg.1 

thank you so much for your response and supporting me. Yes, I have update few inputs  in "lwipopts.h" file but i am currently not sure about the configuration. It would be really appreciated if there is any standard configuration for Lwip Ethernet that works with stm32f746NGHS discovery board.  Pleae 

 
/* USER CODE BEGIN 1 */
#define LWIP_TCP 1
#define LWIP_NETCONN 1
//#define LWIP_DHCP 1
#define LWIP_DNS 1 // handy for MQTT later
#define LWIP_NETIF_HOSTNAME 1
#define LWIP_MDNS_RESPONDER 1 // mDNS (.local)
#define LWIP_IGMP 1 // required for IPv4 multicast 224.0.0.251
#define LWIP_NETBIOSNS 1 // optional: Windows NetBIOS name
#define LWIP_NUM_NETIF_CLIENT_DATA 1 /* required by mDNS */
#define LWIP_SO_RCVTIMEO 1
#define LWIP_AUTOIP 0
#define LWIP_DHCP_AUTOIP_COOP 0
#define LWIP_MQTT 1
#define TCPIP_THREAD_STACKSIZE 3072
#define DEFAULT_THREAD_STACKSIZE 1536
#define MEM_SIZE 16*1024
#define PBUF_POOL_SIZE 16
#define PBUF_POOL_BUFSIZE 1536
#define LWIP_RAM_HEAP_POINTER 0x2004C140
/* USER CODE END 1 */

 

I am adding screenshots ioc information and manual changes in code for reference for better understanding.

I assume DMA Rx and Tx buffer and DTCM non sharable and non cacheable are causing problem.

Stm32f746 host device updated NET link up but when i tried to ping on laptop I get host unreachable. this is due to DMA bufferes are not recognized or dont have memory is not handled properly.

Any further suggestions would be really appreciated.

 

rviswa_0-1759156084786.pngrviswa_1-1759156309617.pngrviswa_2-1759156363392.png

 

rviswa_3-1759156397040.png

rviswaAuthor
Associate
Oct 2, 2025 7:25 AM UTC

Hi @Osman SOYKURT  

@Amel NASRI 

 

Good day!

I am facing a critical issue integrating Ethernet (LWIP) and TouchGFX on my STM32F746NGH Discovery board.

The Problem:
My PC cannot reach the STM32 board over Ethernet. ARP requests fail, resulting in "host unreachable." I understand this is likely due to incorrect memory configuration for the Ethernet DMA and buffers, which require non-cacheable memory regions. I am not familiar with memory mapping before and this helps me to learn and understand how it works in future. I am really appreciated for your valuable inputs. 

My Challenge:
When I modify the MPU settings and linker script to define non-cacheable memory for Ethernet, one of two things happens:

  1. The Ethernet network works (DHCP or static IP), but TouchGFX freezes.

  2. The system crashes with a Hard Fault error.

I need to define separate, non-overlapping memory regions for Ethernet DMA/buffers (non-cacheable) and TouchGFX framebuffers (cacheable) without causing conflicts.

Could a technical expert please help me resolve this memory mapping issue? I would greatly appreciate guidance on the correct MPU configuration and linker script adjustments. The below script doesn't create any hardfault handler erros and no TouchGFX freeze or hand issue but I can't communicate Ethernet(LWIP). 

rviswa_0-1759389655282.pngrviswa_1-1759389673210.png

 

void MPU_Config(void)
{
 MPU_Region_InitTypeDef MPU_InitStruct = {0};

 HAL_MPU_Disable();

 /* SDRAM 0xC0000000 (8 MB): Normal, cacheable, write-through (C=1, B=0) */
 MPU_InitStruct.Enable = MPU_REGION_ENABLE;
 MPU_InitStruct.Number = MPU_REGION_NUMBER0;
 MPU_InitStruct.BaseAddress = 0xC0000000;
 MPU_InitStruct.Size = MPU_REGION_SIZE_8MB;
 MPU_InitStruct.SubRegionDisable = 0x00;
 MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
 MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
 MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
 MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
 MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE; /* C=1 */
 MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; /* B=0 -> WT */
 HAL_MPU_ConfigRegion(&MPU_InitStruct);

 /* QSPI 0x90000000 (16 MB): Normal, cacheable (write-through is fine too) */
 MPU_InitStruct.Number = MPU_REGION_NUMBER1;
 MPU_InitStruct.BaseAddress = 0x90000000;
 MPU_InitStruct.Size = MPU_REGION_SIZE_16MB;
 MPU_InitStruct.SubRegionDisable = 0x00;
 MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
 MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
 MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
 MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
 MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
 MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
 HAL_MPU_ConfigRegion(&MPU_InitStruct);

 HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}

 

/* Entry Point */
ENTRY(Reset_Handler)

/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */

_Min_Heap_Size = 0xa00; /* required amount of heap */
_Min_Stack_Size = 0xa00; /* required amount of stack */

/* Memories definition */
MEMORY
{
 RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K
 FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K
 QUADSPI (r) : ORIGIN = 0x90000000, LENGTH = 16M
 SDRAM (xrw) : ORIGIN = 0xC0000000, LENGTH = 8M
}

/* Sections */
SECTIONS
{

 /* The startup code into "FLASH" Rom type memory */
 .isr_vector :
 {
 . = ALIGN(4);
 KEEP(*(.isr_vector)) /* Startup code */
 . = ALIGN(4);
 } >FLASH

 /* The program code and other data into "FLASH" Rom type memory */
 .text :
 {
 . = ALIGN(4);
 *(.text) /* .text sections (code) */
 *(.text*) /* .text* sections (code) */
 *(.glue_7) /* glue arm to thumb code */
 *(.glue_7t) /* glue thumb to arm code */
 *(.eh_frame)

 KEEP (*(.init))
 KEEP (*(.fini))

 . = ALIGN(4);
 _etext = .; /* define a global symbols at end of code */
 } >FLASH

 /* Constant data into "FLASH" Rom type memory */
 .rodata :
 {
 . = ALIGN(4);
 *(.rodata) /* .rodata sections (constants, strings, etc.) */
 *(.rodata*) /* .rodata* sections (constants, strings, etc.) */
 . = ALIGN(4);
 } >FLASH

 .ARM.extab (READONLY) : /* The "READONLY" keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 . = ALIGN(4);
 *(.ARM.extab* .gnu.linkonce.armextab.*)
 . = ALIGN(4);
 } >FLASH

 .ARM (READONLY) : /* The "READONLY" keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 . = ALIGN(4);
 __exidx_start = .;
 *(.ARM.exidx*)
 __exidx_end = .;
 . = ALIGN(4);
 } >FLASH

 .preinit_array (READONLY) : /* The "READONLY" keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 . = ALIGN(4);
 PROVIDE_HIDDEN (__preinit_array_start = .);
 KEEP (*(.preinit_array*))
 PROVIDE_HIDDEN (__preinit_array_end = .);
 . = ALIGN(4);
 } >FLASH

 .init_array (READONLY) : /* The "READONLY" keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 . = ALIGN(4);
 PROVIDE_HIDDEN (__init_array_start = .);
 KEEP (*(SORT(.init_array.*)))
 KEEP (*(.init_array*))
 PROVIDE_HIDDEN (__init_array_end = .);
 . = ALIGN(4);
 } >FLASH

 .fini_array (READONLY) : /* The "READONLY" keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 . = ALIGN(4);
 PROVIDE_HIDDEN (__fini_array_start = .);
 KEEP (*(SORT(.fini_array.*)))
 KEEP (*(.fini_array*))
 PROVIDE_HIDDEN (__fini_array_end = .);
 . = ALIGN(4);
 } >FLASH

 /* Used by the startup to initialize data */
 _sidata = LOADADDR(.data);

 /* Initialized data sections into "RAM" Ram type memory */
 .data :
 {
 . = ALIGN(4);
 _sdata = .; /* create a global symbol at data start */
 *(.data) /* .data sections */
 *(.data*) /* .data* sections */
 *(.RamFunc) /* .RamFunc sections */
 *(.RamFunc*) /* .RamFunc* sections */

 . = ALIGN(4);
 _edata = .; /* define a global symbol at data end */

 } >RAM AT> FLASH

 /* Uninitialized data section into "RAM" Ram type memory */
 . = ALIGN(4);
 .bss :
 {
 /* This is used by the startup in order to initialize the .bss section */
 _sbss = .; /* define a global symbol at bss start */
 __bss_start__ = _sbss;
 *(.bss)
 *(.bss*)
 *(COMMON)

 . = ALIGN(4);
 _ebss = .; /* define a global symbol at bss end */
 __bss_end__ = _ebss;
 } >RAM


 /* User_heap_stack section, used to check that there is enough "RAM" Ram type memory left */
 ._user_heap_stack :
 {
 . = ALIGN(8);
 PROVIDE ( end = . );
 PROVIDE ( _end = . );
 . = . + _Min_Heap_Size;
 . = . + _Min_Stack_Size;
 . = ALIGN(8);
 } >RAM
 
 /* Remove information from the compiler libraries */
 /DISCARD/ :
 {
 libc.a ( * )
 libm.a ( * )
 libgcc.a ( * )
 }

 .ARM.attributes 0 : { *(.ARM.attributes) } 
 
 /* >>> Custom sections here <<< */
 BufferSection (NOLOAD) :
 {
 *(TouchGFX_Framebuffer TouchGFX_Framebuffer.*) 
 . = ALIGN(4);
	
 } >SDRAM
 
 ExtFlashSection :
 {
 *(ExtFlashSection ExtFlashSection.*) 
 . = ALIGN(4);
 } >QUADSPI
 
 /* Fonts & Texts into QSPI */ 
 FontFlashSection :
 {
 *(FontFlashSection FontFlashSection.*) 
 	. = ALIGN(4);
 } >QUADSPI

 TextFlashSection :
 {
 *(TextFlashSection TextFlashSection.*) 
 	. = ALIGN(4);
 } >QUADSPI

 
 TouchGFX_ScratchbufferA (NOLOAD) :
 {
 *(TouchGFX_ScratchbufferA TouchGFX_ScratchbufferA.*) 	
 	. = ALIGN(4);
 } >SDRAM
 
 TouchGFX_ScratchbufferB (NOLOAD) :
 {
 *(TouchGFX_ScratchbufferB TouchGFX_ScratchbufferB.*) 
 	. = ALIGN(4);
 } >SDRAM 


 
 
}

Please ask me if you need any inputs I can share and update.

 

The below images wherer i have update my memory for DTCM, SRAM1 and SRAM2 at the end either the TougchGFX freeze or hard fault error or sometime i can't run other applicaitons 

rviswa_2-1759389778731.png

rviswa_3-1759389794159.png

 

 

Thank you.