Skip to main content
MGous
Visitor II
Sep 20, 2019 8:39 AM UTC
Question

Error while running GraphApplication

I am trying to implement the Graph widget ( 

http://sw-center.st.com/touchgfx/TouchGFX/Community/GraphApplication.zip

) in touchGFX but i am getting the following error,

The imported project ".\touchgfx\4.8.0\touchgfx\config\msvs\touchgfx_sdl2.props" was not found. Confirm that the path in the <Import> declaration is correct, and that the file exists on disk.

I am using VS 2017 and touchGFX 4.10

This topic has been closed for replies.

1 reply

Martin KJELDSEN
Principal III
Sep 20, 2019 12:37 PM UTC

Hi @MGous​,

Try upgrading the project to 4.10.0 (open it in the designer). It is based on 4.8.0, as is, in the zip file and is not maintained across versions.

/Martin