Skip to main content
Visitor II
May 15, 2025 2:32 PM UTC
Question

Error in TouchGFX 4.25 integration in CubeIDE 1.16.0

After adding in the .ioc file, in software package, Touch GFX and enabled grafic applications. when I try  to lunch ApplicationTemplate.touchgfx.part i receive the following error message. Brlow i also put the content of the log file

 

Sorry - something unexpected has happened which caused an error to occur in the Designer.

For more information, see the log file located at: C:\Users\vdalessandro\AppData\Roaming\TouchGFX-4.25.0\TouchGFXDesigner.log

Please consider reporting this bug and steps to reproduce it at the TouchGFX Help Center so it can be fixed in a future version.
You can find the Help Center here: https://community.st.com/touchgfx

Error: Object reference not set to an instance of an object.

2025-05-15 10:35:12,492 [1] ERROR TouchGFXDesigner.App: Object reference not set to an instance of an object.
System.NullReferenceException: Object reference not set to an instance of an object.
at TouchGFXDesigner.Main.Project.Configuration.FeatureConfig.FeatureConfigCategory.UncheckFeaturesBasedOnSTMFamily(IEnumerable`1 allFeatures, String family, String subFamily)
at TouchGFXDesigner.Main.Project.Configuration.FeatureConfig.FeatureConfigCategory.InitializeFeatureGroups()
at TouchGFXDesigner.Main.MainWindowViewModel.InitializeFeatureGroupsWhenCreatingNewProject()
at TouchGFXDesigner.Main.MainWindowViewModel.LoadApplication(LoadApplicationEvent loadApplicationEvent)
at ApplicationEvents.ApplicationEvent.Raise[T](T args)
at TouchGFXDesigner.Main.MainWindowViewModel.ViewLoaded(FileInfo file)
at TouchGFXDesigner.Main.MainWindow.MainView_OnLoaded(Object sender, RoutedEventArgs e)
This topic has been closed for replies.

1 reply

Senior III
May 16, 2025 6:39 AM UTC

You need to open the file with extensions .touchgfx, not the .touchgfx.part

Also, please use the "code formatter" here to format your LOG in the post, to make the conversation more clear