Skip to main content
AKovy
Associate
May 19, 2022 7:04 AM UTC
Question

Error in IAR after create project TouchGFX 4.19.1. First compilation after creating simple project for srm32f746g-disco/

Hi All.

  'C:/TouchGFXProjects/MyApplication_1/Middlewares/Third_Party/FreeRTOS/Source/portable/IAR/ARM_CM4F/port.c', needed by 'C:/TouchGFXProjects/MyApplication_1/EWARM/STM32F429I-EVAL/Obj/Middlewares/FreeRTOS/port.o', missing and no known rule to make it         

Subj in question.

This topic has been closed for replies.

16 replies

Andrew Neil
Super User
May 19, 2022 8:30 AM UTC

The error message tells you clearly: it needs the file 'C:/TouchGFXProjects/MyApplication_1/Middlewares/Third_Party/FreeRTOS/Source/portable/IAR/ARM_CM4F/port.c', and it can't find it.

So have you checked that this file does actually exist, and is actually in that location.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AKovy
AKovyAuthor
Associate
May 19, 2022 9:09 AM UTC

File exist but in another folder

c:\TouchGFXProjects\MyApplication_1\Middlewares\Third_Party\FreeRTOS\Source\portable\GCC\ARM_CM7\r0p1\

Andrew Neil
Super User
May 19, 2022 9:56 AM UTC

So you obviously need to fix that, then!

You have two choices:

  1. Move the file to the expected location;
  2. Change the expected location to match the actual location.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AKovy
AKovyAuthor
Associate
May 19, 2022 10:10 AM UTC

I think that the error is in the creation of the IAR project file. In CubeIDE compilation runs without errors

Andrew Neil
Super User
May 19, 2022 10:18 AM UTC

so you need to fix the IAR project file, then.

Was the IAR project file auto-generated by Cube?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AKovy
AKovyAuthor
Associate
May 19, 2022 10:26 AM UTC

This iar project file generated by TouchGFX desiner 4.19.1

AKovy
AKovyAuthor
Associate
May 19, 2022 1:55 PM UTC

c:\TouchGFXProjects\MyApplication\Middlewares\Third_Party\FreeRTOS\Source\portable\GCC\ARM_CM4F\port.c

Proceeding from by the location and name of the directory, the port.c file is intended for CubeIDE(GCC)..

Developers should pay attention to this

Osman SOYKURT
ST Technical Moderator
May 23, 2022 7:59 AM UTC

Hello AKovy,

I tried to reproduce the bug but everything is working fine on my side. Which version of IAR are you using ?

What is your "Min version" on STM32CubeMX when you generate code ?

If you have a specific scenario to reproduce your bug please say to us, so we can have a deeper investigation.

/Osman

ST Software Developer | TouchGFX
AKovy
AKovyAuthor
Associate
May 24, 2022 4:22 AM UTC

Hello.

My version CubeMX is 6.5.0 But I didn't use it

I did as described in this section of the documentation.. Part "Checking memory usage"

https://support.touchgfx.com/4.15/docs/basic-concepts/memory-usage

I create simple project for stm32f746g-disco generate it and compiled by IAR 9.2 and

receive error as lower.

 'C:/TouchGFXProjects/MyApplication_1/Middlewares/Third_Party/FreeRTOS/Source/portable/IAR/ARM_CM4F/port.c', needed by 'C:/TouchGFXProjects/MyApplication_1/EWARM/STM32F429I-EVAL/Obj/Middlewares/FreeRTOS/port.o', missing and no known rule to make it       

Best regards.

Andrew Neil
Super User
May 24, 2022 8:48 AM UTC

I think you need to describe, in detail, the steps you took to create the project.

Try creating a new project, and recording your steps (you could use screenshots).

If you then get the same problem, you have the steps for other people to reproduce it;

If you don't get the same problem, then there must have been some mistake in your first attempt.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.