Skip to main content
NKieg.1
Associate III
March 11, 2021
Solved

Dynamic Graph Scroll Mode decrease in Performance

Hello everyone,

I am quite well set up on my project using an STM32F469I-Disco and TouchGFX. Everything is working very well. However, I would like to display data using a dynamic graph. If I choose a mode different from the Scroll mode, everything is updating very well. But when the dynamic graph is in scroll mode it is lagging quite a bit (~1fps) and the touch is almost not responding. How can I improve the performance in my project?

Thank you everyone !

This topic has been closed for replies.
Alexandre RENOUX
Alexandre RENOUXBest answer
Visitor II
March 15, 2021

Hello NKieg.1,

This problem has already been raised in the community. The development team will have a look at it.

Here is the thread in question (that you are already aware of) : https://community.st.com/s/question/0D53W00000TIAV4SAP/touchgfx-dynamic-graph-widget-scroll-mode-performance-issue

I will close this thread to avoid redundancy. Thank you for your feedback.

/Alexandre

3 replies

Romain DIELEMAN
ST Employee
March 12, 2021

Hi,

Do you also face this issue with the simulator or only on the board ? Would you have a project you could share facing this issue ?

/Romain

Alexandre RENOUX
Alexandre RENOUXBest answer
Visitor II
March 15, 2021

Hello NKieg.1,

This problem has already been raised in the community. The development team will have a look at it.

Here is the thread in question (that you are already aware of) : https://community.st.com/s/question/0D53W00000TIAV4SAP/touchgfx-dynamic-graph-widget-scroll-mode-performance-issue

I will close this thread to avoid redundancy. Thank you for your feedback.

/Alexandre

NKieg.1
NKieg.1Author
Associate III
March 15, 2021

Yes no problem, I will keep checking the other thread then ! Thanks.