Skip to main content
ikassma
Associate III
May 8, 2019 4:40 PM UTC
Question

dynamic graph in touchGFX?

I want to express the value of 0x000000 ~ 0xFFFFFF in real time graph.

The graph of the currently provided demo code should continuously update the entire graph, but I want to show the cumulative data. I want to update the last data continuously like the FIFO function.

​

do you have any idea?​@Martin KJELDSEN​ 

This topic has been closed for replies.

4 replies

Martin KJELDSEN
Principal III
May 16, 2019 12:55 PM UTC

@ikassma​,

Can you give a bit more information about this?`You want to show comulative data, but only the last data. So basically you would require a redraw of the entire graph (potentially) ?

ikassma
ikassmaAuthor
Associate III
May 20, 2019 12:36 AM UTC

@Martin KJELDSEN​ 

hm...

I want to show the ADC data of the signal inputted at 20Hz To in real time without setting the specific time.

​I modified the Graph example to discard the first input data, input the second data into the first buffer, and receive and update the last data. However, the problem with this graph is that it is difficult to construct an automatic scale. If the value suddenly becomes bigger or smaller, Graph does not work.

BPeda
Associate II
Jun 14, 2019 9:27 AM UTC

i want graph from this attached data these are y values